Mass Storage Class SCSI Inquiry Structure.
More...
#include <MassStorageClassCommon.h>
Type define for a SCSI Inquiry structure. Structures of this type are filled out by the device via the MS_Host_GetInquiryData() function, retrieving the attached device's information.
For details of the structure contents, refer to the SCSI specifications.
| uint8_t SCSI_Inquiry_Response_t::AdditionalLength |
| unsigned SCSI_Inquiry_Response_t::AERC |
| unsigned SCSI_Inquiry_Response_t::CmdQue |
| unsigned SCSI_Inquiry_Response_t::DeviceType |
| unsigned SCSI_Inquiry_Response_t::Linked |
| unsigned SCSI_Inquiry_Response_t::NormACA |
| unsigned SCSI_Inquiry_Response_t::PeripheralQualifier |
| uint8_t SCSI_Inquiry_Response_t::ProductID[16] |
| unsigned SCSI_Inquiry_Response_t::RelAddr |
| unsigned SCSI_Inquiry_Response_t::Removable |
| unsigned SCSI_Inquiry_Response_t::Reserved |
| unsigned SCSI_Inquiry_Response_t::Reserved2 |
| uint8_t SCSI_Inquiry_Response_t::Reserved3[2] |
| unsigned SCSI_Inquiry_Response_t::Reserved4 |
| unsigned SCSI_Inquiry_Response_t::ResponseDataFormat |
| uint8_t SCSI_Inquiry_Response_t::RevisionID[4] |
| unsigned SCSI_Inquiry_Response_t::SoftReset |
| unsigned SCSI_Inquiry_Response_t::Sync |
| unsigned SCSI_Inquiry_Response_t::TrmTsk |
| uint8_t SCSI_Inquiry_Response_t::VendorID[8] |
| uint8_t SCSI_Inquiry_Response_t::Version |
| unsigned SCSI_Inquiry_Response_t::WideBus16Bit |
| unsigned SCSI_Inquiry_Response_t::WideBus32Bit |
The documentation for this struct was generated from the following file: