Mass Storage Class SCSI Sense Structure.
More...
#include <MassStorageClassCommon.h>
Type define for a SCSI Sense structure. Structures of this type are filled out by the device via the MS_Host_RequestSense() function, indicating the current sense data of the device (giving explicit error codes for the last issued command). For details of the structure contents, refer to the SCSI specifications.
| uint8_t SCSI_Request_Sense_Response_t::AdditionalLength |
| uint8_t SCSI_Request_Sense_Response_t::AdditionalSenseCode |
| uint8_t SCSI_Request_Sense_Response_t::AdditionalSenseQualifier |
| uint8_t SCSI_Request_Sense_Response_t::CmdSpecificInformation[4] |
| unsigned SCSI_Request_Sense_Response_t::EOM |
| uint8_t SCSI_Request_Sense_Response_t::FieldReplaceableUnitCode |
| unsigned SCSI_Request_Sense_Response_t::FileMark |
| unsigned SCSI_Request_Sense_Response_t::ILI |
| uint8_t SCSI_Request_Sense_Response_t::Information[4] |
| unsigned SCSI_Request_Sense_Response_t::Reserved |
| uint8_t SCSI_Request_Sense_Response_t::ResponseCode |
| uint8_t SCSI_Request_Sense_Response_t::SegmentNumber |
| unsigned SCSI_Request_Sense_Response_t::SenseKey |
| uint8_t SCSI_Request_Sense_Response_t::SenseKeySpecific[3] |
The documentation for this struct was generated from the following file: