Audio class-specific Streaming Audio Interface Descriptor (LUFA naming conventions). More...
#include <AudioClassCommon.h>
Data Fields | |
| uint16_t | AudioFormat |
| uint8_t | FrameDelay |
| USB_Descriptor_Header_t | Header |
| uint8_t | Subtype |
| uint8_t | TerminalLink |
Type define for an Audio class-specific streaming interface descriptor. This indicates to the host how audio streams within the device are formatted. See the USB Audio specification for more details.
| uint16_t USB_Audio_Descriptor_Interface_AS_t::AudioFormat |
Format of the audio stream, see Audio Device Formats specification.
| uint8_t USB_Audio_Descriptor_Interface_AS_t::FrameDelay |
Delay in frames resulting from the complete sample processing from input to output.
| USB_Descriptor_Header_t USB_Audio_Descriptor_Interface_AS_t::Header |
Regular descriptor header containing the descriptor's type and length.
| uint8_t USB_Audio_Descriptor_Interface_AS_t::Subtype |
Sub type value used to distinguish between audio class-specific descriptors, a value from the Audio_CSInterface_AS_SubTypes_t enum.
| uint8_t USB_Audio_Descriptor_Interface_AS_t::TerminalLink |
ID value of the output terminal this descriptor is describing.