Audio class-specific Extended Endpoint Descriptor (LUFA naming conventions). More...
#include <AudioClassCommon.h>
Data Fields | |
| uint8_t | Attributes |
| USB_Descriptor_Header_t | Header |
| uint16_t | LockDelay |
| uint8_t | LockDelayUnits |
| uint8_t | Subtype |
Type define for an Audio class-specific extended endpoint descriptor. This contains extra information on the usage of endpoints used to stream audio in and out of the USB Audio device, and follows an Audio class-specific extended endpoint descriptor. See the USB Audio specification for more details.
| uint8_t USB_Audio_Descriptor_StreamEndpoint_Spc_t::Attributes |
Audio class-specific endpoint attributes, such as AUDIO_EP_FULL_PACKETS_ONLY.
| USB_Descriptor_Header_t USB_Audio_Descriptor_StreamEndpoint_Spc_t::Header |
Regular descriptor header containing the descriptor's type and length.
| uint16_t USB_Audio_Descriptor_StreamEndpoint_Spc_t::LockDelay |
Time required to internally lock endpoint's internal clock recovery circuitry.
| uint8_t USB_Audio_Descriptor_StreamEndpoint_Spc_t::LockDelayUnits |
Units used for the LockDelay field, see Audio class specification.
| uint8_t USB_Audio_Descriptor_StreamEndpoint_Spc_t::Subtype |
Sub type value used to distinguish between audio class-specific descriptors, a value from the Audio_CSEndpoint_SubTypes_t enum.