Audio class-specific Streaming Endpoint Descriptor (LUFA naming conventions). More...
#include <AudioClassCommon.h>
Data Fields | |
| USB_Descriptor_Endpoint_t | Endpoint |
| uint8_t | Refresh |
| uint8_t | SyncEndpointNumber |
Type define for an Audio class-specific endpoint descriptor. This contains a regular endpoint descriptor with a few Audio-class-specific extensions. See the USB Audio specification for more details.
| USB_Descriptor_Endpoint_t USB_Audio_Descriptor_StreamEndpoint_Std_t::Endpoint |
Standard endpoint descriptor describing the audio endpoint.
| uint8_t USB_Audio_Descriptor_StreamEndpoint_Std_t::Refresh |
Always set to zero for Audio class devices.
| uint8_t USB_Audio_Descriptor_StreamEndpoint_Std_t::SyncEndpointNumber |
Endpoint address to send synchronization information to, if needed (zero otherwise).