24-Bit Audio Frequency Structure. More...
#include <AudioClassCommon.h>
Data Fields | |
| uint8_t | Byte1 |
| uint8_t | Byte2 |
| uint8_t | Byte3 |
Type define for a 24-bit audio sample frequency structure. As GCC does not contain a built in 24-bit datatype, this this structure is used to build up the value instead. Fill this structure with the AUDIO_SAMPLE_FREQ() macro.
| uint8_t USB_Audio_SampleFreq_t::Byte1 |
Lowest 8 bits of the 24-bit value.
| uint8_t USB_Audio_SampleFreq_t::Byte2 |
Middle 8 bits of the 24-bit value.
| uint8_t USB_Audio_SampleFreq_t::Byte3 |
Upper 8 bits of the 24-bit value.