Audio class-specific Format Descriptor (USB-IF naming conventions). More...
#include <AudioClassCommon.h>
Data Fields | |
| uint8_t | bBitResolution |
| uint8_t | bDescriptorSubtype |
| uint8_t | bDescriptorType |
| uint8_t | bFormatType |
| uint8_t | bLength |
| uint8_t | bNrChannels |
| uint8_t | bSampleFrequencyType |
| uint8_t | bSubFrameSize |
Type define for an Audio class-specific audio format descriptor. This is used to give the host full details about the number of channels, the sample resolution, acceptable sample frequencies and encoding method used in the device's audio streams. See the USB Audio specification for more details.
| uint8_t USB_Audio_StdDescriptor_Format_t::bBitResolution |
Bits of resolution of each channel's samples in the stream.
| uint8_t USB_Audio_StdDescriptor_Format_t::bDescriptorSubtype |
Sub type value used to distinguish between audio class-specific descriptors, a value from the Audio_CSInterface_AS_SubTypes_t enum.
| uint8_t USB_Audio_StdDescriptor_Format_t::bDescriptorType |
Sub type value used to distinguish between audio class-specific descriptors, must be AUDIO_DSUBTYPE_CSInterface_FormatType.
| uint8_t USB_Audio_StdDescriptor_Format_t::bFormatType |
Format of the audio stream, see Audio Device Formats specification.
| uint8_t USB_Audio_StdDescriptor_Format_t::bLength |
Size of the descriptor, in bytes.
| uint8_t USB_Audio_StdDescriptor_Format_t::bNrChannels |
Total number of discrete channels in the stream.
| uint8_t USB_Audio_StdDescriptor_Format_t::bSampleFrequencyType |
Total number of sample frequencies supported by the device. When zero, this must be followed by the lower and upper continuous sampling frequencies supported by the device; otherwise, this must be followed by the given number of discrete sampling frequencies supported.
| uint8_t USB_Audio_StdDescriptor_Format_t::bSubFrameSize |
Size in bytes of each channel's sample data in the stream.