Audio class-specific Extended Endpoint Descriptor (USB-IF naming conventions). More...
#include <AudioClassCommon.h>
Data Fields | |
| uint8_t | bDescriptorSubtype |
| uint8_t | bDescriptorType |
| uint8_t | bLength |
| uint8_t | bLockDelayUnits |
| uint8_t | bmAttributes |
| uint16_t | wLockDelay |
Type define for an Audio class-specific extended endpoint descriptor. This contains extra information on the usage of endpoints used to stream audio in and out of the USB Audio device, and follows an Audio class-specific extended endpoint descriptor. See the USB Audio specification for more details.
| uint8_t USB_Audio_StdDescriptor_StreamEndpoint_Spc_t::bDescriptorSubtype |
Sub type value used to distinguish between audio class-specific descriptors, a value from the Audio_CSEndpoint_SubTypes_t enum.
| uint8_t USB_Audio_StdDescriptor_StreamEndpoint_Spc_t::bDescriptorType |
Type of the descriptor, either a value in USB_DescriptorTypes_t or a value given by the specific class.
| uint8_t USB_Audio_StdDescriptor_StreamEndpoint_Spc_t::bLength |
Size of the descriptor, in bytes.
| uint8_t USB_Audio_StdDescriptor_StreamEndpoint_Spc_t::bLockDelayUnits |
Units used for the LockDelay field, see Audio class specification.
| uint8_t USB_Audio_StdDescriptor_StreamEndpoint_Spc_t::bmAttributes |
Audio class-specific endpoint attributes, such as AUDIO_EP_FULL_PACKETS_ONLY.
| uint16_t USB_Audio_StdDescriptor_StreamEndpoint_Spc_t::wLockDelay |
Time required to internally lock endpoint's internal clock recovery circuitry.