Audio class-specific Streaming Endpoint Descriptor (USB-IF naming conventions). More...
#include <AudioClassCommon.h>
Data Fields | |
| uint8_t | bDescriptorType |
| uint8_t | bEndpointAddress |
| uint8_t | bInterval |
| uint8_t | bLength |
| uint8_t | bmAttributes |
| uint8_t | bRefresh |
| uint8_t | bSynchAddress |
| uint16_t | wMaxPacketSize |
Type define for an Audio class-specific endpoint descriptor. This contains a regular endpoint descriptor with a few Audio-class-specific extensions. See the USB Audio specification for more details.
| uint8_t USB_Audio_StdDescriptor_StreamEndpoint_Std_t::bDescriptorType |
Type of the descriptor, either a value in USB_DescriptorTypes_t or a value given by the specific class.
| uint8_t USB_Audio_StdDescriptor_StreamEndpoint_Std_t::bEndpointAddress |
Logical address of the endpoint within the device for the current configuration, including direction mask.
| uint8_t USB_Audio_StdDescriptor_StreamEndpoint_Std_t::bInterval |
Polling interval in milliseconds for the endpoint if it is an INTERRUPT or ISOCHRONOUS type.
| uint8_t USB_Audio_StdDescriptor_StreamEndpoint_Std_t::bLength |
Size of the descriptor, in bytes.
| uint8_t USB_Audio_StdDescriptor_StreamEndpoint_Std_t::bmAttributes |
Endpoint attributes, comprised of a mask of the endpoint type (EP_TYPE_*) and attributes (ENDPOINT_ATTR_*) masks.
| uint8_t USB_Audio_StdDescriptor_StreamEndpoint_Std_t::bRefresh |
Always set to zero for Audio class devices.
| uint8_t USB_Audio_StdDescriptor_StreamEndpoint_Std_t::bSynchAddress |
Endpoint address to send synchronization information to, if needed (zero otherwise).
| uint16_t USB_Audio_StdDescriptor_StreamEndpoint_Std_t::wMaxPacketSize |
Size of the endpoint bank, in bytes. This indicates the maximum packet size that the endpoint can receive at a time.