CDC class-specific Functional ACM Descriptor (LUFA naming conventions). More...
#include <CDCClassCommon.h>
Data Fields | |
| uint8_t | Capabilities |
| USB_Descriptor_Header_t | Header |
| uint8_t | Subtype |
Type define for a CDC class-specific functional ACM descriptor. This indicates to the host that the CDC interface supports the CDC ACM subclass of the CDC specification. See the CDC class specification for more details.
| uint8_t USB_CDC_Descriptor_FunctionalACM_t::Capabilities |
Capabilities of the ACM interface, given as a bit mask. For most devices, this should be set to a fixed value of 0x06 - for other capabilities, refer to the CDC ACM specification.
| USB_Descriptor_Header_t USB_CDC_Descriptor_FunctionalACM_t::Header |
Regular descriptor header containing the descriptor's type and length.
| uint8_t USB_CDC_Descriptor_FunctionalACM_t::Subtype |
Sub type value used to distinguish between CDC class-specific descriptors, must be CDC_DSUBTYPE_CSInterface_ACM.