CDC class-specific Functional Header Descriptor (LUFA naming conventions). More...
#include <CDCClassCommon.h>
Data Fields | |
| uint16_t | CDCSpecification |
| USB_Descriptor_Header_t | Header |
| uint8_t | Subtype |
Type define for a CDC class-specific functional header descriptor. This indicates to the host that the device contains one or more CDC functional data descriptors, which give the CDC interface's capabilities and configuration. See the CDC class specification for more details.
| uint16_t USB_CDC_Descriptor_FunctionalHeader_t::CDCSpecification |
Version number of the CDC specification implemented by the device, encoded in BCD format.
| USB_Descriptor_Header_t USB_CDC_Descriptor_FunctionalHeader_t::Header |
Regular descriptor header containing the descriptor's type and length.
| uint8_t USB_CDC_Descriptor_FunctionalHeader_t::Subtype |
Sub type value used to distinguish between CDC class-specific descriptors, must be CDC_DSUBTYPE_CSInterface_Header.