CDC class-specific Functional Header Descriptor (USB-IF naming conventions). More...
#include <CDCClassCommon.h>
Data Fields | |
| uint16_t | bcdCDC |
| uint8_t | bDescriptorSubType |
| uint8_t | bDescriptorType |
| uint8_t | bFunctionLength |
Type define for a CDC class-specific functional header descriptor. This indicates to the host that the device contains one or more CDC functional data descriptors, which give the CDC interface's capabilities and configuration. See the CDC class specification for more details.
| uint16_t USB_CDC_StdDescriptor_FunctionalHeader_t::bcdCDC |
Version number of the CDC specification implemented by the device, encoded in BCD format.
| uint8_t USB_CDC_StdDescriptor_FunctionalHeader_t::bDescriptorSubType |
Sub type value used to distinguish between CDC class-specific descriptors, must be CDC_DSUBTYPE_CSInterface_Header.
| uint8_t USB_CDC_StdDescriptor_FunctionalHeader_t::bDescriptorType |
Type of the descriptor, either a value in USB_DescriptorTypes_t or a value given by the specific class.
| uint8_t USB_CDC_StdDescriptor_FunctionalHeader_t::bFunctionLength |
Size of the descriptor, in bytes.