CDC Class Device Mode Configuration and State Structure. More...
#include <CDCClassDevice.h>
Data Fields | |
| struct { | |
| uint8_t ControlInterfaceNumber | |
| USB_Endpoint_Table_t DataINEndpoint | |
| USB_Endpoint_Table_t DataOUTEndpoint | |
| USB_Endpoint_Table_t NotificationEndpoint | |
| } | Config |
| struct { | |
| struct { | |
| uint16_t DeviceToHost | |
| uint16_t HostToDevice | |
| } ControlLineStates | |
| CDC_LineEncoding_t LineEncoding | |
| } | State |
Class state structure. An instance of this structure should be made for each CDC interface within the user application, and passed to each of the CDC class driver functions as the CDCInterfaceInfo parameter. This stores each CDC interface's configuration and state information.
| struct { ... } USB_ClassInfo_CDC_Device_t::Config |
Config data for the USB class interface within the device. All elements in this section must be set or the interface will fail to enumerate and operate correctly.
| uint8_t USB_ClassInfo_CDC_Device_t::ControlInterfaceNumber |
Interface number of the CDC control interface within the device.
| struct { ... } USB_ClassInfo_CDC_Device_t::ControlLineStates |
Current states of the virtual serial port's control lines between the device and host.
| USB_Endpoint_Table_t USB_ClassInfo_CDC_Device_t::DataINEndpoint |
Data IN endpoint configuration table.
| USB_Endpoint_Table_t USB_ClassInfo_CDC_Device_t::DataOUTEndpoint |
Data OUT endpoint configuration table.
| uint16_t USB_ClassInfo_CDC_Device_t::DeviceToHost |
Control line states from the device to host, as a set of CDC_CONTROL_LINE_IN_* masks - to notify the host of changes to these values, call the CDC_Device_SendControlLineStateChange() function.
| uint16_t USB_ClassInfo_CDC_Device_t::HostToDevice |
Control line states from the host to device, as a set of CDC_CONTROL_LINE_OUT_* masks. This value is updated each time CDC_Device_USBTask() is called.
| CDC_LineEncoding_t USB_ClassInfo_CDC_Device_t::LineEncoding |
Line encoding used in the virtual serial port, for the device's information. This is generally only used if the virtual serial port data is to be reconstructed on a physical UART.
| USB_Endpoint_Table_t USB_ClassInfo_CDC_Device_t::NotificationEndpoint |
Notification IN Endpoint configuration table.
| struct { ... } USB_ClassInfo_CDC_Device_t::State |
State data for the USB class interface within the device. All elements in this section are reset to their defaults when the interface is enumerated.