CDC Class Host Mode Configuration and State Structure. More...
#include <CDCClassHost.h>
Data Fields | |
| struct { | |
| USB_Pipe_Table_t DataINPipe | |
| USB_Pipe_Table_t DataOUTPipe | |
| USB_Pipe_Table_t NotificationPipe | |
| } | Config |
| struct { | |
| uint8_t ControlInterfaceNumber | |
| struct { | |
| uint16_t DeviceToHost | |
| uint16_t HostToDevice | |
| } ControlLineStates | |
| bool IsActive | |
| CDC_LineEncoding_t LineEncoding | |
| } | State |
Class state structure. An instance of this structure should be made within the user application, and passed to each of the CDC class driver functions as the CDCInterfaceInfo parameter. This stores each CDC interface's configuration and state information.
| struct { ... } USB_ClassInfo_CDC_Host_t::Config |
Config data for the USB class interface within the device. All elements in this section must be set or the interface will fail to enumerate and operate correctly.
| uint8_t USB_ClassInfo_CDC_Host_t::ControlInterfaceNumber |
Interface index of the CDC-ACM control interface within the attached device.
| struct { ... } USB_ClassInfo_CDC_Host_t::ControlLineStates |
Current states of the virtual serial port's control lines between the device and host.
| USB_Pipe_Table_t USB_ClassInfo_CDC_Host_t::DataINPipe |
Data IN Pipe configuration table.
| USB_Pipe_Table_t USB_ClassInfo_CDC_Host_t::DataOUTPipe |
Data OUT Pipe configuration table.
| uint16_t USB_ClassInfo_CDC_Host_t::DeviceToHost |
Control line states from the device to host, as a set of CDC_CONTROL_LINE_IN_* masks. This value is updated each time CDC_Host_USBTask() is called.
| uint16_t USB_ClassInfo_CDC_Host_t::HostToDevice |
Control line states from the host to device, as a set of CDC_CONTROL_LINE_OUT_* masks - to notify the device of changes to these values, call the CDC_Host_SendControlLineStateChange() function.
| bool USB_ClassInfo_CDC_Host_t::IsActive |
Indicates if the current interface instance is connected to an attached device, valid after CDC_Host_ConfigurePipes() is called and the Host state machine is in the Configured state.
| CDC_LineEncoding_t USB_ClassInfo_CDC_Host_t::LineEncoding |
Line encoding used in the virtual serial port, for the device's information. This is generally only used if the virtual serial port data is to be reconstructed on a physical UART. When set by the host application, the CDC_Host_SetLineEncoding() function must be called to push the changes to the device.
| USB_Pipe_Table_t USB_ClassInfo_CDC_Host_t::NotificationPipe |
Notification IN Pipe configuration table.
| struct { ... } USB_ClassInfo_CDC_Host_t::State |
State data for the USB class interface within the device. All elements in this section may be set to initial values, but may also be ignored to default to sane values when the interface is enumerated.