HID Class Host Mode Configuration and State Structure. More...
#include <HIDClassHost.h>
Data Fields | |
| struct { | |
| USB_Pipe_Table_t DataINPipe | |
| USB_Pipe_Table_t DataOUTPipe | |
| uint8_t HIDInterfaceProtocol | |
| HID_ReportInfo_t * HIDParserData | |
| } | Config |
| struct { | |
| bool DeviceUsesOUTPipe | |
| uint16_t HIDReportSize | |
| uint8_t InterfaceNumber | |
| bool IsActive | |
| uint8_t LargestReportSize | |
| bool SupportsBootProtocol | |
| bool UsingBootProtocol | |
| } | State |
Class state structure. An instance of this structure should be made within the user application, and passed to each of the HID class driver functions as the HIDInterfaceInfo parameter. This stores each HID interface's configuration and state information.
| struct { ... } USB_ClassInfo_HID_Host_t::Config |
Config data for the USB class interface within the device. All elements in this section must be set or the interface will fail to enumerate and operate correctly.
| USB_Pipe_Table_t USB_ClassInfo_HID_Host_t::DataINPipe |
Data IN Pipe configuration table.
| USB_Pipe_Table_t USB_ClassInfo_HID_Host_t::DataOUTPipe |
Data OUT Pipe configuration table.
| bool USB_ClassInfo_HID_Host_t::DeviceUsesOUTPipe |
Indicates if the current interface instance uses a separate OUT data pipe for OUT reports, or if OUT reports are sent via the control pipe instead.
| uint8_t USB_ClassInfo_HID_Host_t::HIDInterfaceProtocol |
HID interface protocol value to match against if a specific boot subclass protocol is required, a protocol value from the HID_Descriptor_ClassSubclassProtocol_t enum.
| HID_ReportInfo_t* USB_ClassInfo_HID_Host_t::HIDParserData |
HID parser data to store the parsed HID report data, when boot protocol is not used.
HID_HOST_BOOT_PROTOCOL_ONLY compile time token is defined, this field is unavailable. | uint16_t USB_ClassInfo_HID_Host_t::HIDReportSize |
Size in bytes of the HID report descriptor in the device.
| uint8_t USB_ClassInfo_HID_Host_t::InterfaceNumber |
Interface index of the HID interface within the attached device.
| bool USB_ClassInfo_HID_Host_t::IsActive |
Indicates if the current interface instance is connected to an attached device, valid after HID_Host_ConfigurePipes() is called and the Host state machine is in the Configured state.
| uint8_t USB_ClassInfo_HID_Host_t::LargestReportSize |
Largest report the device will send, in bytes.
| struct { ... } USB_ClassInfo_HID_Host_t::State |
State data for the USB class interface within the device. All elements in this section may be set to initial values, but may also be ignored to default to sane values when the interface is enumerated.
| bool USB_ClassInfo_HID_Host_t::SupportsBootProtocol |
Indicates if the current interface instance supports the HID Boot Protocol when enabled via HID_Host_SetBootProtocol().
| bool USB_ClassInfo_HID_Host_t::UsingBootProtocol |
Indicates that the interface is currently initialized in Boot Protocol mode