MIDI Class Device Mode Configuration and State Structure. More...
#include <MIDIClassDevice.h>
Data Fields | |
| struct { | |
| USB_Endpoint_Table_t DataINEndpoint | |
| USB_Endpoint_Table_t DataOUTEndpoint | |
| uint8_t StreamingInterfaceNumber | |
| } | Config |
| struct { | |
| uint8_t RESERVED | |
| } | State |
Class state structure. An instance of this structure should be made for each MIDI interface within the user application, and passed to each of the MIDI class driver functions as the MIDIInterfaceInfo parameter. This stores each MIDI interface's configuration and state information.
| struct { ... } USB_ClassInfo_MIDI_Device_t::Config |
Config data for the USB class interface within the device. All elements in this section must be set or the interface will fail to enumerate and operate correctly.
| USB_Endpoint_Table_t USB_ClassInfo_MIDI_Device_t::DataINEndpoint |
Data IN endpoint configuration table.
| USB_Endpoint_Table_t USB_ClassInfo_MIDI_Device_t::DataOUTEndpoint |
Data OUT endpoint configuration table.
| uint8_t USB_ClassInfo_MIDI_Device_t::RESERVED |
| struct { ... } USB_ClassInfo_MIDI_Device_t::State |
State data for the USB class interface within the device. All elements in this section are reset to their defaults when the interface is enumerated.
| uint8_t USB_ClassInfo_MIDI_Device_t::StreamingInterfaceNumber |
Index of the Audio Streaming interface within the device this structure controls.