RNDIS Class Host Mode Configuration and State Structure. More...
#include <RNDISClassHost.h>
Data Fields | |
| struct { | |
| USB_Pipe_Table_t DataINPipe | |
| USB_Pipe_Table_t DataOUTPipe | |
| uint32_t HostMaxPacketSize | |
| USB_Pipe_Table_t NotificationPipe | |
| } | Config |
| struct { | |
| uint8_t ControlInterfaceNumber | |
| uint32_t DeviceMaxPacketSize | |
| bool IsActive | |
| uint32_t RequestID | |
| } | State |
Class state structure. An instance of this structure should be made within the user application, and passed to each of the RNDIS class driver functions as the RNDISInterfaceInfo parameter. This stores each RNDIS interface's configuration and state information.
| struct { ... } USB_ClassInfo_RNDIS_Host_t::Config |
Config data for the USB class interface within the device. All elements in this section must be set or the interface will fail to enumerate and operate correctly.
| uint8_t USB_ClassInfo_RNDIS_Host_t::ControlInterfaceNumber |
Interface index of the RNDIS control interface within the attached device.
| USB_Pipe_Table_t USB_ClassInfo_RNDIS_Host_t::DataINPipe |
Data IN Pipe configuration table.
| USB_Pipe_Table_t USB_ClassInfo_RNDIS_Host_t::DataOUTPipe |
Data OUT Pipe configuration table.
| uint32_t USB_ClassInfo_RNDIS_Host_t::DeviceMaxPacketSize |
Maximum size of a packet which can be buffered by the attached RNDIS device.
| uint32_t USB_ClassInfo_RNDIS_Host_t::HostMaxPacketSize |
Maximum size of a packet which can be buffered by the host.
| bool USB_ClassInfo_RNDIS_Host_t::IsActive |
Indicates if the current interface instance is connected to an attached device, valid after RNDIS_Host_ConfigurePipes() is called and the Host state machine is in the Configured state.
| USB_Pipe_Table_t USB_ClassInfo_RNDIS_Host_t::NotificationPipe |
Notification IN Pipe configuration table.
| uint32_t USB_ClassInfo_RNDIS_Host_t::RequestID |
Request ID counter to give a unique ID for each command/response pair.
| struct { ... } USB_ClassInfo_RNDIS_Host_t::State |
State data for the USB class interface within the device. All elements in this section may be set to initial values, but may also be ignored to default to sane values when the interface is enumerated.