Standard USB Configuration Descriptor (LUFA naming conventions). More...
#include <StdDescriptors.h>
Data Fields | |
| uint8_t | ConfigAttributes |
| uint8_t | ConfigurationNumber |
| uint8_t | ConfigurationStrIndex |
| USB_Descriptor_Header_t | Header |
| uint8_t | MaxPowerConsumption |
| uint16_t | TotalConfigurationSize |
| uint8_t | TotalInterfaces |
Type define for a standard Configuration Descriptor header. This structure uses LUFA-specific element names to make each element's purpose clearer.
| uint8_t USB_Descriptor_Configuration_Header_t::ConfigAttributes |
Configuration attributes, comprised of a mask of USB_CONFIG_ATTR_* masks. On all devices, this should include USB_CONFIG_ATTR_RESERVED at a minimum.
| uint8_t USB_Descriptor_Configuration_Header_t::ConfigurationNumber |
Configuration index of the current configuration.
| uint8_t USB_Descriptor_Configuration_Header_t::ConfigurationStrIndex |
Index of a string descriptor describing the configuration.
| USB_Descriptor_Header_t USB_Descriptor_Configuration_Header_t::Header |
Descriptor header, including type and size.
| uint8_t USB_Descriptor_Configuration_Header_t::MaxPowerConsumption |
Maximum power consumption of the device while in the current configuration, calculated by the USB_CONFIG_POWER_MA() macro.
| uint16_t USB_Descriptor_Configuration_Header_t::TotalConfigurationSize |
Size of the configuration descriptor header, and all sub descriptors inside the configuration.
| uint8_t USB_Descriptor_Configuration_Header_t::TotalInterfaces |
Total number of interfaces in the configuration.