Standard USB Endpoint Descriptor (LUFA naming conventions). More...
#include <StdDescriptors.h>
Data Fields | |
| uint8_t | Attributes |
| uint8_t | EndpointAddress |
| uint16_t | EndpointSize |
| USB_Descriptor_Header_t | Header |
| uint8_t | PollingIntervalMS |
Type define for a standard Endpoint Descriptor. This structure uses LUFA-specific element names to make each element's purpose clearer.
| uint8_t USB_Descriptor_Endpoint_t::Attributes |
Endpoint attributes, comprised of a mask of the endpoint type (EP_TYPE_*) and attributes (ENDPOINT_ATTR_*) masks.
| uint8_t USB_Descriptor_Endpoint_t::EndpointAddress |
Logical address of the endpoint within the device for the current configuration, including direction mask.
| uint16_t USB_Descriptor_Endpoint_t::EndpointSize |
Size of the endpoint bank, in bytes. This indicates the maximum packet size that the endpoint can receive at a time.
| USB_Descriptor_Header_t USB_Descriptor_Endpoint_t::Header |
Descriptor header, including type and size.
| uint8_t USB_Descriptor_Endpoint_t::PollingIntervalMS |
Polling interval in milliseconds for the endpoint if it is an INTERRUPT or ISOCHRONOUS type.