Standard USB Interface Association Descriptor (LUFA naming conventions). More...
#include <StdDescriptors.h>
Data Fields | |
| uint8_t | Class |
| uint8_t | FirstInterfaceIndex |
| USB_Descriptor_Header_t | Header |
| uint8_t | IADStrIndex |
| uint8_t | Protocol |
| uint8_t | SubClass |
| uint8_t | TotalInterfaces |
Type define for a standard Interface Association Descriptor. This structure uses LUFA-specific element names to make each element's purpose clearer.
This descriptor has been added as a supplement to the USB2.0 standard, in the ECN located at http://www.usb.org/developers/docs/InterfaceAssociationDescriptor_ecn.pdf. It allows composite devices with multiple interfaces related to the same function to have the multiple interfaces bound together at the point of enumeration, loading one generic driver for all the interfaces in the single function. Read the ECN for more information.
| uint8_t USB_Descriptor_Interface_Association_t::Class |
Interface class ID.
| uint8_t USB_Descriptor_Interface_Association_t::FirstInterfaceIndex |
Index of the first associated interface.
| USB_Descriptor_Header_t USB_Descriptor_Interface_Association_t::Header |
Descriptor header, including type and size.
| uint8_t USB_Descriptor_Interface_Association_t::IADStrIndex |
Index of the string descriptor describing the interface association.
| uint8_t USB_Descriptor_Interface_Association_t::Protocol |
Interface protocol ID.
| uint8_t USB_Descriptor_Interface_Association_t::SubClass |
Interface subclass ID.
| uint8_t USB_Descriptor_Interface_Association_t::TotalInterfaces |
Total number of associated interfaces.