Standard USB Interface Descriptor (LUFA naming conventions). More...
#include <StdDescriptors.h>
Data Fields | |
| uint8_t | AlternateSetting |
| uint8_t | Class |
| USB_Descriptor_Header_t | Header |
| uint8_t | InterfaceNumber |
| uint8_t | InterfaceStrIndex |
| uint8_t | Protocol |
| uint8_t | SubClass |
| uint8_t | TotalEndpoints |
Type define for a standard Interface Descriptor. This structure uses LUFA-specific element names to make each element's purpose clearer.
| uint8_t USB_Descriptor_Interface_t::AlternateSetting |
Alternate setting for the interface number. The same interface number can have multiple alternate settings with different endpoint configurations, which can be selected by the host.
| uint8_t USB_Descriptor_Interface_t::Class |
Interface class ID.
| USB_Descriptor_Header_t USB_Descriptor_Interface_t::Header |
Descriptor header, including type and size.
| uint8_t USB_Descriptor_Interface_t::InterfaceNumber |
Index of the interface in the current configuration.
| uint8_t USB_Descriptor_Interface_t::InterfaceStrIndex |
Index of the string descriptor describing the interface.
| uint8_t USB_Descriptor_Interface_t::Protocol |
Interface protocol ID.
| uint8_t USB_Descriptor_Interface_t::SubClass |
Interface subclass ID.
| uint8_t USB_Descriptor_Interface_t::TotalEndpoints |
Total number of endpoints in the interface.