Standard HID Boot Protocol Keyboard Report. More...
#include <HIDClassCommon.h>
Data Fields | |
| uint8_t | KeyCode [6] |
| uint8_t | Modifier |
| uint8_t | Reserved |
Type define for a standard Boot Protocol Keyboard report
| uint8_t USB_KeyboardReport_Data_t::KeyCode[6] |
Key codes of the currently pressed keys.
| uint8_t USB_KeyboardReport_Data_t::Modifier |
Keyboard modifier byte, indicating pressed modifier keys (a combination of HID_KEYBOARD_MODIFER_* masks).
| uint8_t USB_KeyboardReport_Data_t::Reserved |
Reserved for OEM use, always set to 0.