MIDI class-specific Streaming Interface Descriptor (LUFA naming conventions). More...
#include <MIDIClassCommon.h>
Data Fields | |
| uint16_t | AudioSpecification |
| USB_Descriptor_Header_t | Header |
| uint8_t | Subtype |
| uint16_t | TotalLength |
Type define for an Audio class-specific MIDI streaming interface descriptor. This indicates to the host how MIDI the specification compliance of the device and the total length of the Audio class-specific descriptors. See the USB Audio specification for more details.
| uint16_t USB_MIDI_Descriptor_AudioInterface_AS_t::AudioSpecification |
Binary coded decimal value, indicating the supported Audio Class specification version.
| USB_Descriptor_Header_t USB_MIDI_Descriptor_AudioInterface_AS_t::Header |
Regular descriptor header containing the descriptor's type and length.
| uint8_t USB_MIDI_Descriptor_AudioInterface_AS_t::Subtype |
Sub type value used to distinguish between audio class-specific descriptors.
| uint16_t USB_MIDI_Descriptor_AudioInterface_AS_t::TotalLength |
Total length of the Audio class-specific descriptors, including this descriptor.