MIDI class-specific Output Jack Descriptor (LUFA naming conventions). More...
#include <MIDIClassCommon.h>
Data Fields | |
| USB_Descriptor_Header_t | Header |
| uint8_t | JackID |
| uint8_t | JackStrIndex |
| uint8_t | JackType |
| uint8_t | NumberOfPins |
| uint8_t | SourceJackID [1] |
| uint8_t | SourcePinID [1] |
| uint8_t | Subtype |
Type define for an Audio class-specific MIDI OUT jack. This gives information to the host on a MIDI output, either a physical output jack, or a logical jack (sending output data internally, or to the host via an endpoint).
| USB_Descriptor_Header_t USB_MIDI_Descriptor_OutputJack_t::Header |
Regular descriptor header containing the descriptor's type and length.
| uint8_t USB_MIDI_Descriptor_OutputJack_t::JackID |
ID value of this jack - must be a unique value within the device.
| uint8_t USB_MIDI_Descriptor_OutputJack_t::JackStrIndex |
Index of a string descriptor describing this descriptor within the device.
| uint8_t USB_MIDI_Descriptor_OutputJack_t::JackType |
Type of jack, one of the JACKTYPE_* mask values.
| uint8_t USB_MIDI_Descriptor_OutputJack_t::NumberOfPins |
Number of output channels within the jack, either physical or logical.
| uint8_t USB_MIDI_Descriptor_OutputJack_t::SourceJackID[1] |
ID of each output pin's source data jack.
| uint8_t USB_MIDI_Descriptor_OutputJack_t::SourcePinID[1] |
Pin number in the input jack of each output pin's source data.
| uint8_t USB_MIDI_Descriptor_OutputJack_t::Subtype |
Sub type value used to distinguish between audio class-specific descriptors.