MIDI class-specific Streaming Interface Descriptor (USB-IF naming conventions). More...
#include <MIDIClassCommon.h>
Data Fields | |
| uint16_t | bcdMSC |
| uint8_t | bDescriptorSubtype |
| uint8_t | bDescriptorType |
| uint8_t | bLength |
| uint16_t | wTotalLength |
Type define for an Audio class-specific MIDI streaming interface descriptor. This indicates to the host how MIDI the specification compliance of the device and the total length of the Audio class-specific descriptors. See the USB Audio specification for more details.
| uint16_t USB_MIDI_StdDescriptor_AudioInterface_AS_t::bcdMSC |
Binary coded decimal value, indicating the supported MIDI Class specification version.
| uint8_t USB_MIDI_StdDescriptor_AudioInterface_AS_t::bDescriptorSubtype |
Sub type value used to distinguish between audio class-specific descriptors.
| uint8_t USB_MIDI_StdDescriptor_AudioInterface_AS_t::bDescriptorType |
Type of the descriptor, either a value in USB_DescriptorTypes_t or a value given by the specific class.
| uint8_t USB_MIDI_StdDescriptor_AudioInterface_AS_t::bLength |
Size of the descriptor, in bytes.
| uint16_t USB_MIDI_StdDescriptor_AudioInterface_AS_t::wTotalLength |
Total length of the Audio class-specific descriptors, including this descriptor.