MIDI class-specific Output Jack Descriptor (USB-IF naming conventions). More...
#include <MIDIClassCommon.h>
Data Fields | |
| uint8_t | baSourceID [1] |
| uint8_t | baSourcePin [1] |
| uint8_t | bDescriptorSubtype |
| uint8_t | bDescriptorType |
| uint8_t | bJackID |
| uint8_t | bJackType |
| uint8_t | bLength |
| uint8_t | bNrInputPins |
| uint8_t | iJack |
Type define for an Audio class-specific MIDI OUT jack. This gives information to the host on a MIDI output, either a physical output jack, or a logical jack (sending output data internally, or to the host via an endpoint).
| uint8_t USB_MIDI_StdDescriptor_OutputJack_t::baSourceID[1] |
ID of each output pin's source data jack.
| uint8_t USB_MIDI_StdDescriptor_OutputJack_t::baSourcePin[1] |
Pin number in the input jack of each output pin's source data.
| uint8_t USB_MIDI_StdDescriptor_OutputJack_t::bDescriptorSubtype |
Sub type value used to distinguish between audio class-specific descriptors.
| uint8_t USB_MIDI_StdDescriptor_OutputJack_t::bDescriptorType |
Type of the descriptor, either a value in USB_DescriptorTypes_t or a value given by the specific class.
| uint8_t USB_MIDI_StdDescriptor_OutputJack_t::bJackID |
ID value of this jack - must be a unique value within the device.
| uint8_t USB_MIDI_StdDescriptor_OutputJack_t::bJackType |
Type of jack, one of the JACKTYPE_* mask values.
| uint8_t USB_MIDI_StdDescriptor_OutputJack_t::bLength |
Size of the descriptor, in bytes.
| uint8_t USB_MIDI_StdDescriptor_OutputJack_t::bNrInputPins |
Number of output channels within the jack, either physical or logical.
| uint8_t USB_MIDI_StdDescriptor_OutputJack_t::iJack |
Index of a string descriptor describing this descriptor within the device.