Standard USB Control Request. More...
#include <StdRequestType.h>
Data Fields | |
| uint8_t | bmRequestType |
| uint8_t | bRequest |
| uint16_t | wIndex |
| uint16_t | wLength |
| uint16_t | wValue |
Type define for a standard USB control request.
| uint8_t USB_Request_Header_t::bmRequestType |
Type of the request.
| uint8_t USB_Request_Header_t::bRequest |
Request command code.
| uint16_t USB_Request_Header_t::wIndex |
wIndex parameter of the request.
| uint16_t USB_Request_Header_t::wLength |
Length of the data to transfer in bytes.
| uint16_t USB_Request_Header_t::wValue |
wValue parameter of the request.