Standard USB Configuration Descriptor (USB-IF naming conventions). More...
#include <StdDescriptors.h>
Data Fields | |
| uint8_t | bConfigurationValue |
| uint8_t | bDescriptorType |
| uint8_t | bLength |
| uint8_t | bmAttributes |
| uint8_t | bMaxPower |
| uint8_t | bNumInterfaces |
| uint8_t | iConfiguration |
| uint16_t | wTotalLength |
Type define for a standard Configuration Descriptor header. This structure uses the relevant standard's given element names to ensure compatibility with the standard.
| uint8_t USB_StdDescriptor_Configuration_Header_t::bConfigurationValue |
Configuration index of the current configuration.
| uint8_t USB_StdDescriptor_Configuration_Header_t::bDescriptorType |
Type of the descriptor, either a value in USB_DescriptorTypes_t or a value given by the specific class.
| uint8_t USB_StdDescriptor_Configuration_Header_t::bLength |
Size of the descriptor, in bytes.
| uint8_t USB_StdDescriptor_Configuration_Header_t::bmAttributes |
Configuration attributes, comprised of a mask of USB_CONFIG_ATTR_* masks. On all devices, this should include USB_CONFIG_ATTR_RESERVED at a minimum.
| uint8_t USB_StdDescriptor_Configuration_Header_t::bMaxPower |
Maximum power consumption of the device while in the current configuration, calculated by the USB_CONFIG_POWER_MA() macro.
| uint8_t USB_StdDescriptor_Configuration_Header_t::bNumInterfaces |
Total number of interfaces in the configuration.
| uint8_t USB_StdDescriptor_Configuration_Header_t::iConfiguration |
Index of a string descriptor describing the configuration.
| uint16_t USB_StdDescriptor_Configuration_Header_t::wTotalLength |
Size of the configuration descriptor header, and all sub descriptors inside the configuration.