Standard USB Descriptor Header (USB-IF naming conventions). More...
#include <StdDescriptors.h>
Data Fields | |
| uint8_t | bDescriptorType |
| uint8_t | bLength |
Type define for all descriptors' standard header, indicating the descriptor's length and type. This structure uses the relevant standard's given element names to ensure compatibility with the standard.
| uint8_t USB_StdDescriptor_Header_t::bDescriptorType |
Type of the descriptor, either a value in USB_DescriptorTypes_t or a value given by the specific class.
| uint8_t USB_StdDescriptor_Header_t::bLength |
Size of the descriptor, in bytes.