Silicon Laboratories CAN Bootloader Release 0.1, Release Notes
Copyright (C) 2010 Silicon Laboratories, Inc.


Relevant Devices:
-----------------

C8051F500 MCU Family
 

This release contains the following components:
-----------------------------------------------

    * Master MCU Bootloader firmware source and pre-built hex file
    * Target MCU Bootloader firmware source and pre-built hex file
    * Target MCU Example Application firmware source (ver 1 and ver 1.1) and pre-built hex files
    - DemoSteps.txt - step-by-step demonstration instructions
    - ReleaseNotes.txt (this file)

Note:
The PC software "Silicon Labs Serial Bootloader Data Source" source code (Visual C#) 
and installer (setup.exe) are included as part of AN533SW.zip. This software is required for 
this bootloader framework. 
This can be downloaded from: http://www.silabs.com/products/mcu/Pages/ApplicationNotes.aspx

Release Dates
-------------
	CAN Bootloader Version 0.1 - November 29, 2010


Silicon Laboratories CAN Bootloader Revision History
----------------------------------------------------


Version 0.1
	New Features/Enhancements
	-------------------------
	Initial release. 


	Corrections
	-----------
	None.