MCU Production Programmer Release 4.85 Release Notes Copyright (C) 2021 Silicon Laboratories, Inc. This release contains the following components: * MCU Production Programmer * MCU Production Programmer Source Files * Communication Dll's * Release Notes (this file) Notes ----- 1. If the programmed hex file locks the Flash of the MCU, The MCU Production Programmer will not be able to serialize the device. Release Dates ------------- Production Programmer Version 4.85 - October 24, 2021 Production Programmer Version 4.81 - July 22, 2019 Production Programmer Version 4.80 - June 14, 2019 Production Programmer Version 4.10 - June 15, 2018 Production Programmer Version 4.00 - January 9, 2018 Production Programmer Version 3.90 - December 19, 2017 Production Programmer Version 3.80 - December 6, 2017 Production Programmer Version 3.70 - December 21, 2016 Production Programmer Version 3.50 - January 25, 2016 Production Programmer Version 3.40 - November 2, 2015 Production Programmer Version 3.10 - November 1, 2013 Production Programmer Version 3.01 - July 31, 2013 Production Programmer Version 3.00 - June 19, 2013 Production Programmer Version 2.90 - July 15, 2012 Production Programmer Version 2.82 - June 15, 2012 Production Programmer Version 2.80 - December 20, 2011 Production Programmer Version 2.70 - December 7, 2011 Production Programmer Version 2.50 - March 1, 2011 Production Programmer Version 2.40 - October 26, 2010 Production Programmer Version 2.30 - August 3, 2010 Production Programmer Version 2.20 - June 30, 2010 Production Programmer Version 2.10 - March 1, 2010 Production Programmer Version 2.00 - October 28, 2009 Production Programmer Version 1.9 - June 3, 2009 Production Programmer Version 1.8 - April 27, 2009 Production Programmer Version 1.7 - March 2, 2009 Production Programmer Version 1.6 - October 8, 2008 Production Programmer Version 1.5 - September 8, 2008 Production Programmer Version 1.4 - July 28, 2008 Production Programmer Version 1.3 - July 1, 2008 Production Programmer Version 1.2 - April 15, 2008 Production Programmer Version 1.1 - February 25, 2008 Production Programmer Version 1.0 - October 4, 2007 Revision History ---------------- Version 4.82 Updated EFM8BB4x, EFM8BB5x OPN support. Version 4.81 Support added for EFM8BB10F4I-QFN20 & EFM8BB10F2I-QFN20. Version 4.80 Rebuild using V4.80 SiUtil.dll. Also added .lib file for source build requirement. Version 4.10 Added support for EFMLB1xFxxES1 derivatives: EFM8LB12F64ES1-QFN32 EFM8LB12F64ES1-QFN24 EFM8LB12F32ES1-QFN32 EFM8LB12F32ES1-QFN32 EFM8LB11F32ES1-QFN32 EFM8LB11F32ES1-QFN24 EFM8LB11F16ES1-QFN32 EFM8LB11F16ES1-QFN24 EFM8LB10F16ES1-QFN32 EFM8LB10F16ES1-QFN24 Version 4.00 Removed un-supported devices: EFM8BB10F8Y-QSOP24 EFM8BB10F8Y-QFN20 EFM8BB10F8Y-SOIC16 EFM8BB10F4Y-QFN20 EFM8BB10F2Y-QFN20 Version 3.90 Added support for following automotive/industrial EFM8 devices: EFM8SB10F8A-QFN20 EFM8SB10F8A-QFN24 EFM8BB10F8A-QSOP24 EFM8BB10F8A-QFN20 EFM8BB10F8A-SOIC16 EFM8BB10F4A-QSOP24 EFM8BB10F4A-QFN20 EFM8BB10F4A-SOIC16 EFM8BB10F2A-QSOP24 EFM8BB10F2A-QFN20 EFM8BB10F2A-SOIC16 EFM8BB22F16A-QFN28 EFM8BB21F16A-QSOP24 EFM8BB21F16A-QFN20 EFM8BB31F16I-QFN32 EFM8BB31F16I-QFP32 EFM8BB31F16I-QSOP24 EFM8BB31F16I-QFN24 EFM8BB31F64A-5QFN32 EFM8BB31F64A-4QFN24 EFM8BB31F32A-5QFN32 EFM8BB31F32A-4QFN24 EFM8BB31F16A-5QFN32 EFM8BB31F16A-4QFN24 EFM8BB31F64I-5QFN32 EFM8BB31F64I-4QFN24 EFM8BB31F32I-5QFN32 EFM8BB31F32I-4QFN24 EFM8BB31F16I-5QFN32 EFM8BB31F16I-4QFN24 Version 3.80 Added support for EFM8 UB3 devices. Version 3.70 Fixed a problem that caused programming to fail due to part name mis-match caused when certain parts used extended device names. Devices include C8051F85x/86x and C8051F99x-B1. Version 3.50 Added support for EFM8 BB1/BB2/BB3/UB1/UB2/SB1/SB2/LB1 devices. Version 3.40 Fixed unicode bug that caused program crash. Version 3.10 Support added for Si1060/1/2/3/4/5 devices. Support added for Si1080/1/2/3/4/5 devices. Support added for C8051F388/9/A/B/C devices. Version 3.01 Firmware for the Toolstick Adapter has been updated to Version 0x0D. Version 3.00 Support added for C8051F850/1/2/3/4/5-GU/IU-GM/IM and C8051F860/1/2/3/4/5-GS/IS devices. Firmware for the USB Debug Adapter has been updated to Version 0x22. Firmware for the Toolstick Adapter has been updated to Version 0x0C. Firmware for the UDA Adapter has been updated to Version 0x05. Version 2.90 Added support for C8051F370/1/4/5 devices Added support for C8051F390/1/2/3/4/5/6/7/8/9 devices Added support for C8051T626/7 devices Version 2.82 Fixed bug where the programmer would not connect to the adapter. Application code updated to Visual Studio 2010 Version 2.80 Fixed bug in loading older save files where the debug adapter contains a false value. The app will now prompt to select the proper debug adapter. Version 2.70 Support added for C8051F960/1/2/3/4/5/6/7/8/9 Support added for Si1020/1/2/3/4/5/6/7 Support added for Si1030/1/2/3/4/5/6/7 Version 2.60 Support added for C8051F750/1/2, C8051F750B/1B/2B/5B/6B/7B Support added for C8051F760/1/2/5/6/7 Version 2.50 Support added for C8051F380/1/2/3/4/5/6/7 devices Support added for C8051T620/1 and C8051T320/1/2/3 devices Support added for C8051T622/3 and C8051T326/7 devices Version 2.40 Added debug adapter and debug adapter type to the .pgs file. Added Load and Save options to the main dialog menu bar. adding support for Big/Little Endian with the serial number and parts available updating correctly. Updated unicode implementation. Version 2.30 Support added for CP2501 devices Version 2.20 Support added for C8051F980/1/2/3/5/6/7/8/9 devices Support added for C8051F990/1/6/7 devices Support added for C8051F716 & 717 devices. Current serial number is now preserved in the settings file. Option added to program serial number in unicode format. Version 2.10 Support added for Si10xx devices. Version 2.00 Support added for C8051F34C/D devices. Support added for C8051F800/1/2/3/4/5/6/7/8/9 devices. Support added for C8051F810/1/2/3/4/5/6/7/8/9 devices. Support added for C8051F820/1/2/3/4/5/6/7/8/9 devices. Support added for C8051F830/1/2/3/4/5 devices. Support added for C8051F901/2 devices. Support added for C8051F911/2 devices. Version 1.9 Support added for C8051F550/1/2/3/4/5/6/7 devices. Support added for C8051F560/1/2/3/4/5/6/7/8/9 devices. Support added for C8051F570/1/2/3/4/5 devices. Support added for C8051F540/1/2/3/4/5/6/7 devices. Version 1.8 Support added for C8051T606 device. Version 1.7 Support added for C8051F58x/59x devices. Support added for C8051F508/509/510/511 devices. Support added for C8051F70x/71x devices. Version 1.6 Support added for C8051F34A/34B devices. Version 1.5 Firmware for the EC2 Serial Adapter has been updated to Version 22. Firmware for the USB Debug Adapter has been updated to Version 20. Firmware for the Toolstick Adapter has been updated to Version 5. Version 1.4 Support added for C8051F500/1/2/3/4/5/6/7 devices. Version 1.3 Support added for C8051F348/349 devices. Version 1.2 Support added for C8051F52xA/53xA devices. Support added for programming the flash lock byte. Support added for downloading hex files to multiple banks. (F12x/F13x) Support added for 17-bit addressing for serial number code location. Removed Windows hotkeys when the application does not have focus. Added the option to use flash persistence. Changed erase routine to use FLASHErase() functions instead of Download(). Version 1.1 Support added for C8051T630/1/2/3/4/5 devices. Support added for C8051T610/1/2/3/4/5/6/7 devices. Support added for C8051F930/1 devices. Support added for C8051F920/1 devices. Version 1.0 Initial Release