==============================================================
2v0p1
==============================================================

Added Features
 * General improvements for CLI commands.

Addressed issues:
 * Stored PTI configuration would not be applied on boot.

Known Issues/Limitations:
 * VUART on series 2 devices may stop working after a reset of the the target device.


==============================================================
2v0p0
==============================================================

Added Features:
 * Added WinUSB support
     The driver mode will change to WinUSB automatically after the update.
     This will cause the USB PID to change, which may cause issues in special setups relying on the PID.
     For Windows 7 and earlier: Please install the latest SEGGER J-Link software pack
     with the "Legacy drivers" option enabled before installing this update.
     If needed, the mode can be changed back to SEGGER using either one of:
     - Simplicity Commander: "commander adapter drivermode" or GUI
     - Admin console: The "sys drivermode" command.
     - SEGGER J-Link Configurator
 * Enabled PCODE and HSS support

Addressed issues:
 * None

Known Issues/Limitations:
 * VUART on series 2 devices may stop working after a reset of the the target device.


==============================================================
1v6p0
==============================================================

Added Features:
 * Disable VCOM buffers when in debug mode "IN" to allow an external adapter to use the VCOM port
 * Added command to restore default configuration - "sys restore"
 * Added command to manually disable/enable VCOM - "serial vcom enable/disable"
 * Support controlling power on/off from PC tools

Addressed issues:
 * Fixed potential for corrupting configuration
 * Identification of radio boards could fail intermittently
 * Concurrent use of RTT and VCOM could cause data loss on the VCOM channel.
 * Connecting to port 4901 would fail in certain scenarios. Introduced in 1.5.1.
 * Series 1 device recovery was unreliable. Introduced in 1.5.1.

Known Issues/Limitations:
 * VUART on series 2 devices may stop working after a reset of the the target device.


==============================================================
1v5p1
==============================================================

Added Features:
 * Support for VCOM config from PC tools
 * Support starting AEM calibration from PC tools
 * Support for reading and writing scratchpad from PC tools
 * Support reading MAC address from PC tools
 * Support clearing the nickname by using syntax 'sys nickname ""'
 * Updated the base J-Link debugger application sources

Addressed issues:
 * None

Known Issues/Limitations:
 * VUART on series 2 devices may stop working after a reset of the the target device.


==============================================================
1v4p13
==============================================================

Addressed issues:
 * Configuration over SWO could cause VCOM CTS to get stuck high, preventing the target from transmitting any data on VCOM until next reset

Known Issues/Limitations;
 * VUART on EFR32xG22/EFR32xG21 may stop working after a reset of the target device.
 * BCC Packet handling is currently disabled
 * UDP discovery protocol key=value pairs for group "node" not implemented yet


==============================================================
1v4p12
==============================================================

Addressed issues:
 * Debug mode was not restored after boot since 1v4p10. The board would always boot in debug mode MCU, but still appear to be in the stored mode.
 * Fixed VUART on devices with flash base address 0x08000000 (xG24 and newer)
 * For a small set of radio boards, the stored CTUNE values were not exposed to external applications (e.g. Commander/Studio)

Known Issues/Limitations;
 * VUART on EFR32xG22/EFR32xG21 may stop working after a reset of the target device.
 * BCC Packet handling is currently disabled
 * UDP discovery protocol key=value pairs for group "node" not implemented yet


==============================================================
1v4p11
==============================================================

Addressed issues:
 * SWO failed if it was read more than once in a session

Known Issues/Limitations;
 * VUART on EFR32xG22/EFR32xG21 may stop working after a reset of the target device.
 * BCC Packet handling is currently disabled
 * UDP discovery protocol key=value pairs for group "node" not implemented yet


==============================================================
1v4p10
==============================================================

Added Features:
 * Added support for Configuration over SWO for VCOM and PTI settings
 * Increased max VCOM baud rate from 921600 to 3686400
 * Increased maximum PTI packet length from 1024 B to 1950 B
 * When the reset button is pressed, the board controller refreshes the display
 * Added net mac CLI command to show the MAC address
 * Added sys voltage CLI command to check VMCU, 5V, Vtarget and 3V3
 * New PTI mode: VUART over PTI, only applies to Si917
 * The reported maximum target interface speed is now dependent on the type of interface (SWD, JTAG, C2)

Addressed issues:
 * Improved PTI capture stability

Known Issues/Limitations;
 * VUART on EFR32xG22/EFR32xG21 may stop working after a reset of the target device.
 * BCC Packet handling is currently disabled
 * UDP discovery protocol key=value pairs for group "node" not implemented yet


==============================================================
1v4p6
==============================================================

Added Features:
 * Support for configuring PTI baudrate to 3.2MHz. This requires a RAIL version above 2.8.0.13.
 * Added "serial vcom stats" for statistics on VCOM data.

Addressed issues:
 * Ensure that debug interface is properly deinitialized when reading AEM data over USB. This could cause the target device to draw extra current.
 * Reduced current consumption of the kit in some situations.
 * Support for different number of Up and Down-channels for RTT when using VUART.

Known Issues/Limitations;
 * VUART on EFR32xG22/EFR32xG21 may stop working after a reset of the target device.
 * BCC Packet handling is currently disabled
 * UDP discovery protocol key=value pairs for group "node" not implemented yet


==============================================================
1v4p4
==============================================================

Added Features:
 * If the kit firmware crashes, the kit will now automatically reboot.
 * Added "time info" CLI command that will print more info about the time synchronization service.

Addressed issues:
 * VUART does not work over USB. This is now supported when using silink > 0.5.0
 * Fixed an issue where the first bytes of a PTI frame could be lost if the frame, including preamble, lasted for more than 10 ms.
 * Fixed an issue where the WSTK would not always respond to a UDP Discovery packet.
 * Fixed an issue where the kit would sometimes erroneously report that it was not able to start time synchronization in client mode.

Known Issues/Limitations;
 * VUART on EFR32xG22/EFR32xG21 may stop working after a reset of the target device.
 * BCC Packet handling is currently disabled
 * UDP discovery protocol key=value pairs for group "node" not implemented yet


==============================================================
1v4p3
==============================================================

Added Features;
 * Improved kit startup time
 * Error message on the VUART console if the kit is unable to connect to the target device

Addressed Issues;
 * When connecting via IP and using RTT it could happen that the kit crashed if the PC did not exit the controlling process in a clean way
 * When using VUART the connection could drop when resetting the target device
 * When using VUART the connection could drop in some situations when the target application was updated

Known Issues/Limitations;
 * BCC Packet handling is currently disabled
 * UDP discovery protocol key=value pairs for group "node" not implemented yet
 * VUART does not work over USB


==============================================================
1v4p2
==============================================================

Bootloader upgrade to bootloader S1016B version 0v9p1b153.

Added Features;
 * None

Addressed Issues;
 * The kit would halt in the bootloader instead of booting normally if the target application drove both push button GPIOs to GND

Known Issues/Limitations;
 * BCC Packet handling is currently disabled
 * UDP discovery protocol key=value pairs for group "node" not implemented yet


==============================================================
1v4p1
==============================================================
Added Features;
 * None

Addressed Issues;
 * WSTK IP Stack resource depletion if receiving time synchronization packets after role reconfiguration. This can happen when the kit has been configured as a time server, and then is reconfigured as either client or time synchronization is disabled.

Known Issues/Limitations;
 * BCC Packet handling is currently disabled
 * UDP discovery protocol key=value pairs for group "node" not implemented yet


==============================================================
1v4p0
==============================================================
Added Features;
 * Added support for VUART with Cortex-M33.

Addressed Issues;
 * PTI packets longer than 200 bytes were not supported. Increased to 1022 bytes.
 * VCOM hardware handshake signal CTS is no longer driven when hardware handshake is disabled.
 * An incorrect AEM gain channel selection boundary caused all measurements between 590 uA and 1250 uA to be reported as 590 uA.
 * Improved VCOM reliability in situations with slow host computers.
 * Improved response time for UDP discovery packets

Known Issues/Limitations;
 * BCC Packet handling is currently disabled
 * UDP discovery protocol key=value pairs for group "node" not implemented yet


==============================================================
1v3p4
==============================================================
Added Features;
 * Added support for reading out CTUNE value from radio boards

Addressed Issues;
 * Fixed issue where data written to USB CDC VCOM port was sometimes lost
 * Enabling PC samples and/or exceptions in the data channel could cause data corruption and lost data

Known Issues/Limitations;
 * BCC Packet handling is currently disabled
 * UDP discovery protocol key=value pairs for group "node" not implemented yet


==============================================================
1v3p3
==============================================================
Added Features;
 * None

Addressed Issues;
 * It could take up to one second from calling "time client" or "time server" before the change took effect

Known Issues/Limitations;
 * BCC Packet handling is currently disabled
 * UDP discovery protocol key=value pairs for group "node" not implemented yet


==============================================================
1v3p2
==============================================================
Added Features;
 * None

Addressed Issues;
 * Data channel (DCH/IP port 4905) timestamps would occasionally be off by 25.6 seconds

Known Issues/Limitations;
 * BCC Packet handling is currently disabled
 * UDP discovery protocol key=value pairs for group "node" not implemented yet


==============================================================
1v3p1
==============================================================
Added Features;
 * None

Addressed Issues;
 * Data channel (DCH/IP port 4905) PTI timestamps would wrap to negative after one hour
 * Data channel (DCH/IP port 4905) AEM timestamp would occasionally be off by 25.6 seconds
 * When connecting to Data channel, all existing PTI data, PC samples and exceptions are now cleared

Known Issues/Limitations;
 * BCC Packet handling is currently disabled
 * UDP discovery protocol key=value pairs for group "node" not implemented yet


==============================================================
1v3p0
==============================================================
Added Features;
 * None

Addressed Issues;
 * Data channel (DCH/IP port 4905) AEM timestamps were sometimes off by +/- 3.2 ms
 * PC sample packets over DCH could in rare occasions get an invalid length, causing some data to be dropped
 * PTI timestamps were more accurately calibrated and adjusted by 1 us

Known Issues/Limitations;
 * BCC Packet handling is currently disabled
 * UDP discovery protocol key=value pairs for group "node" not implemented yet


==============================================================
1v2p2
==============================================================
Added Features;
 * None

Addressed Issues;
 * Hardware handshake auto-config worked in the wrong direction
   * CTS mode was enabled instead of RTS mode

Known Issues/Limitations;
 * BCC Packet handling is currently disabled
 * UDP discovery protocol key=value pairs for group "node" not implemented yet


==============================================================
1v2p1
==============================================================
Added Features;
 * None

Addressed Issues;
 * Debug mode was always reverted to MCU after restart since version 1.2.0
   * Tools would display the configured mode (e.g. OUT), not the actual one (MCU)
 * When using Segger RTT, other functionality would become slow or unavailable
 * Changed behavior of the VCOM RTS line
   * No longer blocking target TX when nothing is connected to VCOM

Known Issues/Limitations;
 * BCC Packet handling is currently disabled
 * UDP discovery protocol key=value pairs for group "node" not implemented yet


==============================================================
1v2p0
==============================================================
Added Features;
 * Support for energy profiler data over Data Channel (DCH)
   * New protocol message version 3 to support new data sources and
     nanosecond timestamps.
   * Protocol message version 2 supported still supported for packet trace (PTI).
   * AEM, PC samples, exceptions and Packet Trace supported using
     protocol message version 3.
 * "dch message" command set added.
   * Protocol message version select.
     * version 2 is default.
   * Selective control of data sources over DCH.
   * Packet trace (PTI) messages enabled by default.

Addressed Issues;
 * VCOM over EMUCOM didn't work in version 1.1.x and newer.

Known Issues/Limitations;
 * BCC Packet handling is currently disabled
 * UDP discovery protocol key=value pairs for group "node" not implemented yet


==============================================================
1v1p1
==============================================================
Added Features;
 * Cortex-M33 support
 * Display/UI improvements for readibility

Addressed Issues;
 * Board ID detection could stop working due to a concurrency issue

Known Issues/Limitations;
 * USB connections must be explicitly closed, there is no timeout
   * If Silink crashes or is killed, a kit restart may be required to restore connectivity
 * BCC Packet handling is currently disabled
 * UDP discovery protocol key=value pairs for group "node" not implemented yet


==============================================================
1v1p0
==============================================================
Added Features;
 * Added support for Admin Console over USB
 * Added support for Virtual UART over USB

Addressed Issues;
 * None

Known Issues/Limitations;
 * USB connections must be explicitly closed, there is no timeout
   * If Silink crashes or is killed, a kit restart may be required to restore connectivity
 * BCC Packet handling is currently disabled
 * UDP discovery protocol key=value pairs for group "node" not implemented yet


==============================================================
1v0p3
==============================================================
Added Features;
 * None

Addressed Issues;
 * PTI would drop packets if the packet rate increased above about 300 packets per second

Known Issues/Limitations;
 * BCC Packet handling is currently disabled
 * UDP discovery protocol key=value pairs for group "node" not implemented yet


==============================================================
1v0p2
==============================================================
Added Features;
 * Improved vcom port command for configuring hardware handshake
   * "auto" mode uses radio board information to configure for the most common use case. Only EFR32 radio boards are considered.
   * Command syntax: "serial vcom config handshake <disabled/rtscts/rts/cts/auto>"
 * Added VUART support for devices with more than 32 kB RAM

Addressed Issues;
 * It is now possible to revert to handshake autoconfig after modifying the configuration
 * Fixed "debug mode" value in discovery data

Known Issues/Limitations;
 * BCC Packet handling is currently disabled
 * UDP discovery protocol key=value pairs for group "node" not implemented yet


==============================================================
1v0p1
==============================================================
Added Features;
 * PTI support for second channel. Only one capture channel at a time is currently supported.

Addressed Issues;
 * Fixed various issues related to stability
 * Fixed boot problem some kits
 * Fixed PTI issue. Very high packet rates could lock up the firmware.

Known Issues/Limitations;
 * BCC Packet handling is currently disabled
 * UDP discovery protocol key=value pairs for group "node" not implemented yet


==============================================================
1v0p0
==============================================================
Added Features;
 * Updated handshake command set
   * Use command "serial vcom config handshake <disabled/rtscts/rts/cts>" to configure
   * Use command "serial vcom config speed <9600...921600>" to configure

Addressed Issues;
 * VirtualCOM port over sockets and EMUCOM had incorrect RTS default state, which affected HW handshake applications.

Known Issues/Limitations;
 * BCC Packet handling is currently disabled
 * UDP discovery protocol key=value pairs for group "node" not implemented yet


==============================================================
0v15p4
==============================================================
Added Features;
 * Added support for hardware flow control on VCOM port
 * Added support for configurable VCOM baud rate up to 921 600 bps
   * Use command "serial config vcom speed <baud rate> handshake <enable/disable>" to configure

Addressed Issues;
 * None

Known Issues/Limitations;
 * BCC Packet handling is currently disabled
 * UDP discovery protocol key=value pairs for group "node" not implemented yet


==============================================================
0v15p3
==============================================================
Added Features;
 * Improved maximum SWD clock speed from 4 MHz to 8 MHz.
 * Improved SWD stability when debugging external targets.

Addressed Issues;
 * None

Known Issues/Limitations;
 * BCC Packet handling is currently disabled
 * UDP discovery protocol key=value pairs for group "node" not implemented yet


==============================================================
0v15p2
==============================================================
Added Features;
 * Added support for ARTIK Wireless STK.

Addressed Issues;
 * None

Known Issues/Limitations;
 * BCC Packet handling is currently disabled
 * UDP discovery protocol key=value pairs for group "node" not implemented yet


==============================================================
0v15p1
==============================================================
Added Features;
 * Added a feature that will cause a rescan/init of the RAM control block ( RTT ) whenever you connect to the
   IP port 4900 and when a debugger pin reset is issued. This is useful when an application using VirtualUART is
   rebuilt, causing the location of the RAM control block to move.

Addressed Issues;
 * None

Known Issues/Limitations;
 * BCC Packet handling is currently disabled
 * UDP discovery protocol key=value pairs for group "node" not implemented yet


==============================================================
0v15p0
==============================================================
Added Features;
 * Added support for downstream EmberDebug. ( Host -> Target direction ). IP port 4900 will now forward data to the target over
   RTT channel with name "silabsvuartdown".

Addressed Issues;
 * Fixed an isse where occasional data on the upstream VirtualUART channel would get lost if a socket connection to port 4905 was not opened.

Known Issues/Limitations;
 * BCC Packet handling is currently disabled
 * UDP discovery protocol key=value pairs for group "node" not implemented yet


==============================================================
0v14p3
==============================================================
Added Features;
 * Extended board support.
 * Support for persistent discovery key.
 * Improved output from "pti config" command.

Addressed Issues;
 * None

Known Issues/Limitations;
 * BCC Packet handling is currently disabled
 * UDP discovery protocol key=value pairs for group "node" not implemented yet


==============================================================
0v14p2
==============================================================
Added Features;
 * None

Addressed Issues;
 * Fixed kit reset which could occur when using VCOM/Debugger/AEM simultaneously over USB.

Known Issues/Limitations;
 * BCC Packet handling is currently disabled
 * UDP discovery protocol key=value pairs for group "node" not implemented yet


==============================================================
0v14p1
==============================================================
Added Features;
 * Fixed target->WSTK protocol parsing for emberDebug.
 * Added back "serial" command, that was accidentally removed.

Addressed Issues;
 * None

Known Issues/Limitations;
 * BCC Packet handling is currently disabled
 * UDP discovery protocol key=value pairs for group "node" not implemented yet


==============================================================
0v14p0
==============================================================
Added Features;
 * Added support for JTAG.
 * Improved debugger bus SWD/JTAG bus performance by up to 50%.
 * Improved reliability of IP socket connections.
 * Added support for reconnecting to sockets.
 * Packet trace interface (PTI) configuration is now persistent when set using the admin console. This configuration is used when auto-config fails.
 * Default PTI configuration is now EFR32.
 * Support for SWO / Virtual UART in standard CMSIS mode.
 * Support for EmberDebug using SWO
 * Added filter for host debugger use when kit is in debug mode IN. I.e. when using an external debugger, use of the on-board debugger will be filtered.

Addressed Issues;
 * Override serial port configuration to always enable hardware flow control if BRD4301 is detected.

Known Issues/Limitations;
 * BCC Packet handling is currently disabled
 * UDP discovery protocol key=value pairs for group "node" not implemented yet


==============================================================
0v13p2
==============================================================
Added Features;
 * None

Addressed Issues;
 * Override serial port configuration to always enable hardware flow control if any EFR32MG radio board is connected

Known Issues/Limitations;
 * BCC Packet handling is currently disabled
 * UDP discovery protocol key=value pairs for group "node" not implemented yet


==============================================================
0v13p1
==============================================================
Added Features;
 * None

Addressed Issues;
 * Override serial port configuration to always enable hardware flow control if BRD4100 or BRD4300 is connected.

Known Issues/Limitations;
 * BCC Packet handling is currently disabled
 * UDP discovery protocol key=value pairs for group "node" not implemented yet


==============================================================
0v13p0
==============================================================
Added Features;
 * Added serial port configuration command to enable/disable hardware flow control on VCOM port.

Addressed Issues;
 * None

Known Issues/Limitations;
 * BCC Packet handling is currently disabled
 * UDP discovery protocol key=value pairs for group "node" not implemented yet


==============================================================
0v12p1
==============================================================
Added Features;
 * Added visual indication ("sys visual" command)

Addressed Issues;
 * Fixed issue where the measured voltage in AEM and the debugger could be wrong
 * Fixed PTI auto config for EFR32 radio boards
 * Improved handling of socket connections

Known Issues/Limitations;
 * BCC Packet handling is currently disabled
 * UDP discovery protocol key=value pairs for group "node" not implemented yet


==============================================================
0v12p0
==============================================================
Added Features;
 * Enabled SWO printf output on port 4900

Addressed Issues;
 * Fixed issue with AEM calibration which could cause offsets in the measured current.

Known Issues/Limitations;
 * BCC Packet handling is currently disabled
 * UDP discovery protocol key=value pairs for group "node" not implemented yet


==============================================================
0v11p2
==============================================================
Added Features;
 * Enabled PTI0 and VCOM on the Simplicity Connector when in debug OUT or IN mode.

Addressed Issues;
 * Reduced latency in target serial port from ~20 ms to ~2 ms.
 * Fixed issue with AEM calibration which could cause (negative) offsets in the measured current.

Known Issues/Limitations;
 * BCC Packet handling is currently disabled
 * UDP discovery protocol key=value pairs for group "node" not implemented yet


==============================================================
0v11p1
==============================================================
Added Features;
 * Flash page protect and unprotect is supported on EFM32, EZR32 and EFR32.
 * Debug lock / unlock is supported on EFM32 and EZR32.
 * Device recovery of all EFM32, EZR32 devices except EFM32G Gecko is now supported.
   EFM32 Gecko parts can be unlocked if locked, but not recovered in case of GPIO misconfiguration or similar.
   The EFM32-G8xx-STK supports this.
 * Added USB support for PTI data channel packets
 * Packet trace auto-config based on radio board IDs
 * Added support for resetting the target device by sending a break signal over the USB serial port (CDC).
 * New bootloader release 0.9.0 build 89 now follows the firmware package. The bootloader will be upgraded when neccessary.

Addressed Issues;
 * Fixed an issue where data over the USB serial port (CDC) could "get stuck" in firmware buffers
   and not be forwarded until new data arrived.
 * Fixed an issue where firmware could crash when changing debug mode.
 * Fixed an issue when USB host enumeration/connection would fail on some USB hubs and computers.
 * Fixed an issue where the AEM current sampling frequency was incorrectly reported.
   AEM sampling frequency is now 10000 Hz and correctly reported.
 * Fixed incorrect reading of RESET pin which caused J-Link warnings
 * Fixed an issue where repeated data channel socket disconnect/reconnect over port 4905 would fail
   until reboot of the kit.

Known Issues/Limitations;
 * BCC Packet handling is currently disabled
 * UDP discovery protocol key=value pairs for group "node" not implemented yet


==============================================================
0v2p4
==============================================================
Added Features;
 * Improved production test

Addressed Issues;

Known Issues;
 * BCC Packet handling is currently disabled
 * Changing IP address may cause the admin console to become unavailable until the kit is rebooted
 * UDP discovery protocol key=value pairs for group "node" not implemented yet


==============================================================
0v2p1
==============================================================
Added Features;

Addressed Issues;

Known Issues;
 * BCC Packet handling is currently disabled
 * Changing IP address may cause the admin console to become unavailable until the kit is rebooted
 * UDP discovery protocol key=value pairs for group "node" not implemented yet


==============================================================
0v2p0
==============================================================
Added Features;
 * Added packet trace and data channel on port 4905

Addressed Issues;

Known Issues;
 * BCC Packet handling is currently disabled
 * Changing IP address may cause the admin console to become unavailable until the kit is rebooted
 * UDP discovery protocol key=value pairs for group "node" not implemented yet


==============================================================
0v1p7
==============================================================
Added Features;
 * Added "discovery" admin console command that returns the same key-value pairs as the ISD UDP discovery
   protocol.
 * Added support for time syncronization between WSTKs and ISA3 adapters.
 * Added "time" command group to control the TimeSvc task.
 * Added board list to the UDP discovery protocol
 * Fixed some of the UDP discovery key=value pairs that was previously not set.

Addressed Issues;
 * Moved APPDATA EMUCOM channel to (USER + 11).

Known Issues;
 * BCC Packet handling is currently disabled
 * Changing IP address may cause the admin console to become unavailable until the kit is rebooted
 * UDP discovery protocol key=value pairs for group "node" not implemented yet


==============================================================
0v1p6
==============================================================
Added Features;

Addressed Issues;
 * Fixed broken firmware package

Known Issues;
 * BCC Packet handling is currently disabled
 * Changing IP address may cause the admin console to become unavailable until the kit is rebooted


==============================================================
0v1p5
==============================================================
Added Features;
 * SWO is now supported
 * Added discovery
 * Added "sys nickname" command
 * Added "target button" and "target reset" commands
 * Added "quit" command

Addressed Issues;

Known Issues;
 * BCC Packet handling is currently disabled
 * Changing IP address may cause the admin console to become unavailable until the kit is rebooted


==============================================================
0v1p4
==============================================================
Added Features;
 * Added admin console on port 4902
 * Added virtual COM port on port 4901
 * BCC now operates in transparent virtual COM port mode by default

Addressed Issues;

Known Issues;
 * BCC Packet handling is currently disabled
 * Changing IP address may cause the admin console to become unavailable until the kit is rebooted


==============================================================
0v1p3
==============================================================
Added Features;
 * Preliminary support debugging EFM8 devices. Requires J-Link DLL v4.94.
 * Radio Board / Add-on Board Board ID support
 * Automatically releasing the display to the target device on MCU STKs after boot

Addressed Issues;
 * Fixed issue where AEM would return INF current samples


==============================================================
0v1p2
==============================================================
Added BRD5000, BRD5001, BRD5100 and BRD5201 support


==============================================================
0v1p1
==============================================================
Initial release