==============================================================
1v4p8
==============================================================

Added Features;
 * Support for configuring PTI baudrate to 3.2MHz. This requires a RAIL version above 2.8.0.13.
 * Added "serial vcom stats" for statistics on VCOM data.
 * Reduced VCOM latency.
 * Error message on the VUART console if the kit is unable to connect to the target device
 * Improved kit startup time

Addressed Issues;
 * Fixed an issue where the first bytes of a PTI frame could be lost if the frame, including preamble, lasted for more than 10 ms.
 * When using VUART the connection could drop when resetting the target device
 * Ensure that debugger SWD pins are properly deinitialized when not actively debugging. This could cause the target device to draw extra current.
 * Ensure that debugger SWD pins are tristated when in debug mode "off".
 * Support for different number of Up and Down-channels for RTT when using VUART.
 * Fixed a bug where the first PTI-frame after PTI interface reconfiguration was dropped.
 * When using VUART the connection could drop in some situations when the target application was updated

Known Issues/Limitations;
 * BCC Packet handling is currently disabled


==============================================================
1v4p2
==============================================================
Added Features;
 * Hardware flow control is now supported.

Addressed Issues;
 * Removed device reset during debugger boot sequence.
 * PTI packets longer than 200 bytes were not supported. Increased to 1022 bytes.
 * Improved VCOM reliability in situations with slow host computers.

Known Issues/Limitations;
 * BCC Packet handling is currently disabled
 * UDP discovery protocol key=value pairs for group "node" not implemented yet


==============================================================
1v3p3
==============================================================
Added Features;
 * Added support for BRD2207A

Addressed Issues;
 * Miscellaneous timestamp fixes for AEM and PTI data

Known Issues/Limitations;
 * None


==============================================================
1v3p0
==============================================================
Added Features;
 * VUART support using Silink over USB
 * VCOM support using Silink over USB
 * Admin Console support using Silink over USB
 * Data channel support using Silink over USB
  * Packet trace capture support on BRD4166 (Thunderboard Sense 2)
  * PC Samples
  * Exceptions
 * SWO support was added in version 0.4.0

Addressed Issues;
 * None

Known Issues/Limitations;
 * None


==============================================================
0v4p1
==============================================================
Added Features;
 * Added support for BRD5203A

Addressed Issues;
 * None

Known Issues/Limitations;
 * SWO is not supported


==============================================================
0v4p0
==============================================================
Added Features;
 * Added support for BRD4166A

Addressed Issues;
 * None

Known Issues/Limitations;
 * SWO is not supported


==============================================================
0v3p1
==============================================================
Added Features;
 * None

Addressed Issues;
 * Improved MSD flashing stability

Known Issues/Limitations;
 * SWO is not supported


==============================================================
0v3p0
==============================================================
Added Features;
 * Added mbed/MSD flashing support

Addressed Issues;
 * None

Known Issues/Limitations;
 * SWO is not supported


==============================================================
0v2p3
==============================================================
Added Features;
 * Improved max SWD clock speed to 1.5 mHz

Addressed Issues;
 * None

Known Issues/Limitations;
 * SWO is not supported


==============================================================
0v2p2
==============================================================
Added Features;
 * Fixed setting production data on external blank boards

Addressed Issues;
 * None

Known Issues/Limitations;
 * SWO is not supported


==============================================================
0v2p1
==============================================================
Added Features;
 * Added support for auto-generating JLink serial number
 * Initial support for BRD7500

Addressed Issues;
 * None

Known Issues/Limitations;
 * SWO is not supported


==============================================================
0v2p0
==============================================================
Initial release