==============================================================
2v0p1
==============================================================

Added Features:
 * General improvements for CLI commands.

Addressed issues:
 * Stored PTI configuration would not be applied on boot.

Known Issues/Limitations:
 * VUART on series 2 devices may stop working after a reset of the the target device.


==============================================================
2v0p0
==============================================================

Added Features:
 * Added WinUSB support
     The driver mode will change to WinUSB automatically after the update.
     This will cause the USB PID to change, which may cause issues in special setups relying on the PID.
     For Windows 7 and earlier: Please install the latest SEGGER J-Link software pack
     with the "Legacy drivers" option enabled before installing this update.
     If needed, the mode can be changed back to SEGGER using either one of:
     - Simplicity Commander: "commander adapter drivermode" or GUI
     - Admin console: The "sys drivermode" command.
     - SEGGER J-Link Configurator
 * Enabled PCODE and HSS support

Addressed issues:
 * None

Known Issues/Limitations:
 * VUART on series 2 devices may stop working after a reset of the the target device.


==============================================================
1v6p1
==============================================================

Added Features:
 * Re-add prodtest radio commands.

Addressed issues:
 * None

Known Issues/Limitations:
 * VUART on series 2 devices may stop working after a reset of the the target device.


==============================================================
1v6p0
==============================================================

Added Features:
 * Added command to restore default configuration - "sys restore"
 * Added command to manually disable/enable VCOM - "serial vcom enable/disable"
 * Support controlling power on/off and voltage from PC tools
 * Added board support: BRD2606A, BRD2608A, BRD2708A, BRD2709A, BRD2710A, BRD2711A, BRD2713A

Addressed issues:
 * Fixed potential for corrupting configuration
 * Improved resistance against "garbage" UART bytes when VCOM is disabled
 * Concurrent use of RTT and VCOM could cause data loss on the VCOM channel.
 * Series 1 device recovery was unreliable. Introduced in 1.5.1.

Known Issues/Limitations:
 * VUART on series 2 devices may stop working after a reset of the the target device.


==============================================================
1v5p2
==============================================================

Added Features:
 * Power down external flash before entering sleep mode
   * Decreases current draw on BRD2705A and BRD2606A

Addressed issues:
 * None

Known Issues/Limitations:
 * VUART on series 2 devices may stop working after a reset of the the target device.


==============================================================
1v5p1
==============================================================

Added Features:
 * Support for reading and writing scratchpad from PC tools
 * Support clearing the nickname by using syntax 'sys nickname ""'
 * Updated the base J-Link debugger application sources

Addressed issues:
 * Firmware upgrade could fail on some boards (BRD4314A, and all Laird boards)
   * To recover, ground TP999 for a few seconds when connecting power to halt in
     the bootloader, and then upgrade firmware normally

Known Issues/Limitations:
 * VUART on series 2 devices may stop working after a reset of the the target device.


==============================================================
1v5p0
==============================================================

Added Features:
 * Support for "auxillary UART" for SiWx917 devices, re-purposing flow control pins
 * Support for VCOM config from PC tools
 * Support entering ISP mode for SiWx917 devices

Addressed issues:
 * None

Known Issues/Limitations:
 * VUART on series 2 devices may stop working after a reset of the the target device.


==============================================================
1v4p13
==============================================================
Added features:
 * None

Addressed issues:
 * Board ID did not work on BRD2704A, introduced in 1v4p12.
   Affected boards appear as "BRD0000A", and must be recovered using Simplicity Commander 1.16.1 or newer.

Known Issues/Limitations;
 * VUART on series 2 devices may stop working after a reset of the the target device debug interface


==============================================================
1v4p12
==============================================================
Added features:
 * Added support for new boards, including BRD4003A and BRD1015A
 * Increased maximum PTI packet length from 1024 B to 1950 B
 * The reported maximum target interface speed is now dependent on the type of interface (SWD, JTAG, C2)
 * Added "sys voltage" CLI command to check VMCU and 3V3

Addressed issues:
 * VUART didn't work on certain xG24 projects
 * For a small set of radio boards, the stored CTUNE values were not exposed to external applications (e.g. Commander/Studio)

Known Issues/Limitations;
 * VUART on series 2 devices may stop working after a reset of the the target device debug interface


==============================================================
1v4p9
==============================================================
Added features:
 * Added support for new boards

Addressed issues:
 * Stale VUART/SWO data is now flushed when connecting to DCH

Known Issues/Limitations;
 * VUART on series 2 devices may stop working after a reset of the the target device debug interface


==============================================================
1v4p8
==============================================================
Added features:
 * Support for configuring PTI baudrate to 3.2 MHz. This requires a RAIL version above 2.8.0.13.
 * Support for VCOM baudrates up to 3686400 Hz.
 * Reduced VCOM latency.
 * Added "serial vcom stats" for statistics on VCOM data.
 * VUART support for devices with a non-zero flash base address.

Addressed issues:
 * Ensure that debugger SWD pins are properly deinitialized when not actively debugging. This could cause the target device to draw extra current.
 * Ensure that debugger SWD pins are tristated when in either debug mode "in" or "off".
 * Support for different number of Up and Down-channels for RTT when using VUART.
 * Fixed a bug where the first PTI-frame after PTI interface reconfiguration was dropped.
 * Fixed a potential issue where the debugger could draw extra current when powered externally over 5V.

Known Issues/Limitations;
 * VUART on series 2 devices may stop working after a reset of the the target device debug interface


==============================================================
1v4p7
==============================================================
* Support for B variant TB Lynx.
Allows specific testing of new ambient light sensor VEML6035.
* Adding production test support Explorer Kit BGM220.


==============================================================
1v4p6
==============================================================
Support for EFM32PG22 Dev kit


==============================================================
1v4p5
==============================================================
Support for Explorer Kit BGM220


==============================================================
1v4p4
==============================================================
Initial public version

Addressed issues:
 * The kit firmware could in some circumstances report support for AEM
 * The kit firmware could crash when configuring PTI


==============================================================
0v8p0
==============================================================
Initial version