==============================================================
Version 1.3.0
==============================================================

Added Features;
 * Edge now sends capture group info/warning/error messages 
   also via control socket
 * Allow adding/removing devices from an ongoing capture group
   (non-PCAPNG captures only). The capture status of the new
   device will be set to match that of the capture group
 * Added control socket command for reloading JSON state file

Resolved Issues;
 * Changes to the 'serialPort' field of a source in the JSON 
   state file would be overwritten when starting/stopping a 
   capture group
 * Starting a PCAPNG capture to a named pipe/FIFO would fail
   if the named pipe/FIFO already existed

Known Issues;
 * Windows: CTRL-C on "edge capture" stops the capture, but
   does not exit the Edge client. Send CTRL-C again to
   terminate the client.


==============================================================
Version 1.2.1
==============================================================

Added Features;
 * None

Resolved Issues;
 * Fixed control socket handling on Windows.

Known Issues;
 * Windows: CTRL-C on "edge capture" stops the capture, but
   does not exit the Edge client. Send CTRL-C again to
   terminate the client.


==============================================================
Version 1.2.0
==============================================================

Added Features;
 * Added support for 'socket' output mode
 * Added support for switching output modes via control socket

Resolved Issues;
 * None


==============================================================
Version 1.1.0
==============================================================

Added Features;
 * Added 'edge pause' for pausing ongoing captures
 * Added 'edge resume' for resuming paused captures

Resolved Issues;
 * When starting a capture ('edge start'), Edge will no longer
   append data to existing output files; the original file 
   will be moved to a backup location and a new file will be
   created instead
 * Misc stability improvements and bug fixes


==============================================================
Version 1.0.1
==============================================================

Added Features;
 * None

Resolved Issues;
 * Unknown fields in capture group JSON files are no longer 
   overwritten


==============================================================
Version 1.0.0
==============================================================

Added Features;
 * Edge no longer runs as a daemon; the state is kept
   persistantly in a configurable location
 * Added 'edge capture', a one-liner command for starting a 
   capture from one or more sources, which can be stopped by
   sending CTRL+C
 * Aligned Edge with SDM specs for capture interface behavior.
   This includes support for controlling/monitoring capture 
   groups via Unix domain sockets served by Edge

Resolved Issues;
 * None


==============================================================
Version 0.0.5
==============================================================

Added Features;
 * Updated apack.json

Resolved Issues;
 * Index option would fail with start command on Windows


==============================================================
Version 0.0.4
==============================================================

Added Features;
 * Updated start/stop command in apack.json
 * Edge list also prints URL configuration

Resolved Issues;
 * Misc bug fixes


==============================================================
Version 0.0.3
==============================================================

Added Features;
 * Added support to start/stop capture on single devices

Resolved Issues;
 * None


==============================================================
Version 0.0.2
==============================================================

Added Features;
 * Allow groups to be created with given group ID
 * Added "config" command to set a server URL to notify server about status updates

Resolved Issues;
 * Moved --output option to "start" command
 * Improved JSON output