CP21xx Customization Utility v1.2.3 Release Notes
Copyright (C) 2016 Silicon Laboratories, Inc.

KNOWN ISSUES AND LIMITATIONS
----------------------------

    1) Only CP210x, CP211x, and CP213x devices are supported by this
       application.
	
    2) This application does not support automatic refresh of devices.

    3) CP210x is only supported on Linux and Windows
	
    4) CP2130 is only supported on Windows
	
    5) Programming the serial number will display an incorrect failure
       due to improper reset functionality. This will be addressed in a
       future release.
	
    6) Changing the mode from GPIO to modem on a CP2105 will automatically
       change pin settings that don't reflect on the validation. This
       doesn't affect programming specific settings to the device.

Release Dates
-------------

    CP21xx Customization Utility v1.2.3 - Feb 4, 2016
    CP21xx Customization Utility v1.2.2 - December 18 2015
    CP21xx Customization Utility v1.2.1 - November 7, 2014
    CP21xx Customization Utility v1.2.0 - Feb 28, 2014

REVISION HISTORY
-----------------
Version 1.2.3
    Bug fixes for CP2114 programming
    - programming boot config did not work
    - USB strings had two extra null bytes
    - Flush buffers dialog had reversed "RX on open" and "TX on close" bits

Version 1.2.2
    Updated CP2114 programming interface.
    Updated to use latest manufacturing DLL.

Version 1.2.1
    JRE error that occurred when opening the CP21xxCustomizationUtility
    has been fixed.

Version 1.2.0
    Updated to include descriptions in the hex and bit fields
    Fixed bug in CP2130 Port Config write
    Fixed bug in CP2103/4/5 Port Config writes
    Fixed bug in lock values for CP2130/CP2110/CP2114
    Fixed behavior where GPIO/Modem Mode were written seperately and
    incorrectly (combined)

Version 1.1.0
    Added support for CP2130

Version 1.0.1
    Fixed bugs seen when programming CP2105
    Fixed crash when opening on OSX

Version 1.0.0
    Initial Release