Data Structures | |
| struct | PDUAL_PORT_CONFIG |
| struct | _DUAL_PORT_CONFIG |
| CP2105 Dual Port Config Structure. Alias of this struct is DUAL_PORT_CONFIG. More... | |
Macros | |
| #define | PORT_RI_SCI_ON 0x0001 |
| CP2105 Define bit locations for DUAL_PORT_CONFIG.Mode DUAL_PORT_CONFIG.Reset_Latch and DUAL_PORT_CONFIG.Suspend_Latch. More... | |
| #define | PORT_DCD_SCI_ON 0x0002 |
| PORT_DCD_SCI_ON location. More... | |
| #define | PORT_DTR_SCI_ON 0x0004 |
| PORT_DTR_SCI_ON location. More... | |
| #define | PORT_DSR_SCI_ON 0x0008 |
| PORT_DSR_SCI_ON location. More... | |
| #define | PORT_TXD_SCI_ON 0x0010 |
| PORT_TXD_SCI_ON location. More... | |
| #define | PORT_RXD_SCI_ON 0x0020 |
| PORT_RXD_SCI_ON location. More... | |
| #define | PORT_RTS_SCI_ON 0x0040 |
| PORT_RTS_SCI_ON location. More... | |
| #define | PORT_CTS_SCI_ON 0x0080 |
| PORT_CTS_SCI_ON location. More... | |
| #define | PORT_GPIO_0_SCI_ON 0x0002 |
| PORT_GPIO_0_SCI_ON location. More... | |
| #define | PORT_GPIO_1_SCI_ON 0x0004 |
| PORT_GPIO_1_SCI_ON location. More... | |
| #define | PORT_GPIO_2_SCI_ON 0x0008 |
| PORT_GPIO_2_SCI_ON location. More... | |
| #define | PORT_SUSPEND_SCI_ON 0x0001 |
| Can't configure latch value. More... | |
| #define | PORT_RI_ECI_ON 0x0100 |
| PORT_RI_ECI_ON location. More... | |
| #define | PORT_DCD_ECI_ON 0x0200 |
| PORT_DCD_ECI_ON location. More... | |
| #define | PORT_DTR_ECI_ON 0x0400 |
| PORT_DTR_ECI_ON location. More... | |
| #define | PORT_DSR_ECI_ON 0x0800 |
| PORT_DSR_ECI_ON location. More... | |
| #define | PORT_TXD_ECI_ON 0x1000 |
| PORT_TXD_ECI_ON location. More... | |
| #define | PORT_RXD_ECI_ON 0x2000 |
| PORT_RXD_ECI_ON location. More... | |
| #define | PORT_RTS_ECI_ON 0x4000 |
| PORT_RTS_ECI_ON location. More... | |
| #define | PORT_CTS_ECI_ON 0x8000 |
| PORT_CTS_ECI_ON location. More... | |
| #define | PORT_GPIO_0_ECI_ON 0x0400 |
| PORT_GPIO_0_ECI_ON location. More... | |
| #define | PORT_GPIO_1_ECI_ON 0x0800 |
| PORT_GPIO_1_ECI_ON location. More... | |
| #define | PORT_SUSPEND_ECI_ON 0x0100 |
| Can't configure latch value. More... | |
| #define | EF_GPIO_0_TXLED_ECI 0x01 |
| CP2105 Define bit locations for DUAL_PORT_CONFIG.EnhancedFxn_ECI. More... | |
| #define | EF_GPIO_1_RXLED_ECI 0x02 |
| Under device control. More... | |
| #define | EF_GPIO_1_RS485_ECI 0x04 |
| Under device control. More... | |
| #define | EF_INVERT_SUSPEND_ECI 0x10 |
| RS485 Invert bit. More... | |
| #define | EF_DYNAMIC_SUSPEND_ECI 0x40 |
| For GPIO signals. More... | |
| #define | EF_GPIO_0_TXLED_SCI 0x01 |
| CP2105 Define bit locations for DUAL_PORT_CONFIG.EnhancedFxn_SCI. More... | |
| #define | EF_GPIO_1_RXLED_SCI 0x02 |
| Under device control. More... | |
| #define | EF_INVERT_SUSPEND_SCI 0x10 |
| RS485 Invert bit. More... | |
| #define | EF_DYNAMIC_SUSPEND_SCI 0x40 |
| For GPIO signals. More... | |
| #define | EF_WEAKPULLUP 0x10 |
| Weak Pull-up on. More... | |
| #define | EF_WEAKPULLUP 0x10 |
| Weak Pull-up on. More... | |
Dual Port Config definitions see CP210x_GetDualPortConfig() and CP210x_SetDualPortConfig()
| struct DUAL_PORT_CONFIG |
| struct _DUAL_PORT_CONFIG |
CP2105 Dual Port Config Structure. Alias of this struct is DUAL_PORT_CONFIG.
| #define EF_DYNAMIC_SUSPEND_ECI 0x40 |
For GPIO signals.
| #define EF_DYNAMIC_SUSPEND_SCI 0x40 |
For GPIO signals.
| #define EF_GPIO_0_TXLED_ECI 0x01 |
CP2105 Define bit locations for DUAL_PORT_CONFIG.EnhancedFxn_ECI.
Under device control
| #define EF_GPIO_0_TXLED_SCI 0x01 |
CP2105 Define bit locations for DUAL_PORT_CONFIG.EnhancedFxn_SCI.
Under device control
| #define EF_GPIO_1_RS485_ECI 0x04 |
Under device control.
| #define EF_GPIO_1_RXLED_ECI 0x02 |
Under device control.
| #define EF_GPIO_1_RXLED_SCI 0x02 |
Under device control.
| #define EF_INVERT_SUSPEND_ECI 0x10 |
RS485 Invert bit.
| #define EF_INVERT_SUSPEND_SCI 0x10 |
RS485 Invert bit.
| #define EF_WEAKPULLUP 0x10 |
Weak Pull-up on.
CP2105 Define bit locations for DUAL_PORT_CONFIG.EnhancedFxn_Device.
Weak Pull-up on
| #define EF_WEAKPULLUP 0x10 |
Weak Pull-up on.
CP2105 Define bit locations for DUAL_PORT_CONFIG.EnhancedFxn_Device.
Weak Pull-up on
| #define PORT_CTS_ECI_ON 0x8000 |
PORT_CTS_ECI_ON location.
| #define PORT_CTS_SCI_ON 0x0080 |
PORT_CTS_SCI_ON location.
| #define PORT_DCD_ECI_ON 0x0200 |
PORT_DCD_ECI_ON location.
| #define PORT_DCD_SCI_ON 0x0002 |
PORT_DCD_SCI_ON location.
| #define PORT_DSR_ECI_ON 0x0800 |
PORT_DSR_ECI_ON location.
| #define PORT_DSR_SCI_ON 0x0008 |
PORT_DSR_SCI_ON location.
| #define PORT_DTR_ECI_ON 0x0400 |
PORT_DTR_ECI_ON location.
| #define PORT_DTR_SCI_ON 0x0004 |
PORT_DTR_SCI_ON location.
| #define PORT_GPIO_0_ECI_ON 0x0400 |
PORT_GPIO_0_ECI_ON location.
| #define PORT_GPIO_0_SCI_ON 0x0002 |
PORT_GPIO_0_SCI_ON location.
| #define PORT_GPIO_1_ECI_ON 0x0800 |
PORT_GPIO_1_ECI_ON location.
| #define PORT_GPIO_1_SCI_ON 0x0004 |
PORT_GPIO_1_SCI_ON location.
| #define PORT_GPIO_2_SCI_ON 0x0008 |
PORT_GPIO_2_SCI_ON location.
| #define PORT_RI_ECI_ON 0x0100 |
PORT_RI_ECI_ON location.
| #define PORT_RI_SCI_ON 0x0001 |
CP2105 Define bit locations for DUAL_PORT_CONFIG.Mode DUAL_PORT_CONFIG.Reset_Latch and DUAL_PORT_CONFIG.Suspend_Latch.
PORT_RI_SCI_ON location
| #define PORT_RTS_ECI_ON 0x4000 |
PORT_RTS_ECI_ON location.
| #define PORT_RTS_SCI_ON 0x0040 |
PORT_RTS_SCI_ON location.
| #define PORT_RXD_ECI_ON 0x2000 |
PORT_RXD_ECI_ON location.
| #define PORT_RXD_SCI_ON 0x0020 |
PORT_RXD_SCI_ON location.
| #define PORT_SUSPEND_ECI_ON 0x0100 |
Can't configure latch value.
| #define PORT_SUSPEND_SCI_ON 0x0001 |
Can't configure latch value.
| #define PORT_TXD_ECI_ON 0x1000 |
PORT_TXD_ECI_ON location.
| #define PORT_TXD_SCI_ON 0x0010 |
PORT_TXD_SCI_ON location.