Macros | |
| #define | FC_OPEN_TX 0x01 |
| on Open, Tx More... | |
| #define | FC_OPEN_RX 0x02 |
| on Open, Rx More... | |
| #define | FC_CLOSE_TX 0x04 |
| on Close, Tx More... | |
| #define | FC_CLOSE_RX 0x08 |
| on Close, Tx More... | |
| #define | FC_OPEN_TX_SCI FC_OPEN_TX |
| CP2105 - Standard Port. More... | |
| #define | FC_OPEN_RX_SCI FC_OPEN_RX |
| Standard port, on Open, Rx. More... | |
| #define | FC_CLOSE_TX_SCI FC_CLOSE_TX |
| Standard port, on Close, Tx. More... | |
| #define | FC_CLOSE_RX_SCI FC_CLOSE_RX |
| Standard port, on Close, Rx. More... | |
| #define | FC_OPEN_TX_ECI 0x10 |
| CP2105 - Enhanced Port. More... | |
| #define | FC_OPEN_RX_ECI 0x20 |
| Enhanced port, on Open, Tx. More... | |
| #define | FC_CLOSE_TX_ECI 0x40 |
| Enhanced port, on Close, Tx. More... | |
| #define | FC_CLOSE_RX_ECI 0x80 |
| Enhanced port, on Close, Rx. More... | |
| #define | FC_OPEN_TX_IFC0 0x0001 |
| CP2108. More... | |
| #define | FC_OPEN_RX_IFC0 0x0002 |
| CP2108 port 0, on Open, Rx. More... | |
| #define | FC_CLOSE_TX_IFC0 0x0004 |
| CP2108 port 0, on Close, Tx. More... | |
| #define | FC_CLOSE_RX_IFC0 0x0008 |
| CP2108 port 0, on Close, Rx. More... | |
| #define | FC_OPEN_TX_IFC1 0x0010 |
| CP2108 port 1, on Open, Tx. More... | |
| #define | FC_OPEN_RX_IFC1 0x0020 |
| CP2108 port 1, on Open, Rx. More... | |
| #define | FC_CLOSE_TX_IFC1 0x0040 |
| CP2108 port 1, on Close, Tx. More... | |
| #define | FC_CLOSE_RX_IFC1 0x0080 |
| CP2108 port 1, on Close, Rx. More... | |
| #define | FC_OPEN_TX_IFC2 0x0100 |
| CP2108 port 2, on Open, Tx. More... | |
| #define | FC_OPEN_RX_IFC2 0x0200 |
| CP2108 port 2, on Open, Rx. More... | |
| #define | FC_CLOSE_TX_IFC2 0x0400 |
| CP2108 port 2, on Close, Tx. More... | |
| #define | FC_CLOSE_RX_IFC2 0x0800 |
| CP2108 port 2, on Close, Rx. More... | |
| #define | FC_OPEN_TX_IFC3 0x1000 |
| CP2108 port 3, on Open, Tx. More... | |
| #define | FC_OPEN_RX_IFC3 0x2000 |
| CP2108 port 3, on Open, Rx. More... | |
| #define | FC_CLOSE_TX_IFC3 0x4000 |
| CP2108 port 3, on Close, Tx. More... | |
| #define | FC_CLOSE_RX_IFC3 0x8000 |
| CP2108 port 3, on Close, Rx. More... | |
Flush Buffer definitions see CP210x_GetFlushBufferConfig() and CP210x_SetFlushBufferConfig()
When these bits are set, dictate when the device will flush that buffer (TX and/or RX) and upon which event (Open and/or Close)
CP2104
| #define FC_CLOSE_RX 0x08 |
on Close, Tx
| #define FC_CLOSE_RX_ECI 0x80 |
Enhanced port, on Close, Rx.
| #define FC_CLOSE_RX_IFC0 0x0008 |
CP2108 port 0, on Close, Rx.
| #define FC_CLOSE_RX_IFC1 0x0080 |
CP2108 port 1, on Close, Rx.
| #define FC_CLOSE_RX_IFC2 0x0800 |
CP2108 port 2, on Close, Rx.
| #define FC_CLOSE_RX_IFC3 0x8000 |
CP2108 port 3, on Close, Rx.
| #define FC_CLOSE_RX_SCI FC_CLOSE_RX |
Standard port, on Close, Rx.
| #define FC_CLOSE_TX 0x04 |
on Close, Tx
| #define FC_CLOSE_TX_ECI 0x40 |
Enhanced port, on Close, Tx.
| #define FC_CLOSE_TX_IFC0 0x0004 |
CP2108 port 0, on Close, Tx.
| #define FC_CLOSE_TX_IFC1 0x0040 |
CP2108 port 1, on Close, Tx.
| #define FC_CLOSE_TX_IFC2 0x0400 |
CP2108 port 2, on Close, Tx.
| #define FC_CLOSE_TX_IFC3 0x4000 |
CP2108 port 3, on Close, Tx.
| #define FC_CLOSE_TX_SCI FC_CLOSE_TX |
Standard port, on Close, Tx.
| #define FC_OPEN_RX 0x02 |
on Open, Rx
| #define FC_OPEN_RX_ECI 0x20 |
Enhanced port, on Open, Tx.
| #define FC_OPEN_RX_IFC0 0x0002 |
CP2108 port 0, on Open, Rx.
| #define FC_OPEN_RX_IFC1 0x0020 |
CP2108 port 1, on Open, Rx.
| #define FC_OPEN_RX_IFC2 0x0200 |
CP2108 port 2, on Open, Rx.
| #define FC_OPEN_RX_IFC3 0x2000 |
CP2108 port 3, on Open, Rx.
| #define FC_OPEN_RX_SCI FC_OPEN_RX |
Standard port, on Open, Rx.
| #define FC_OPEN_TX 0x01 |
on Open, Tx
| #define FC_OPEN_TX_ECI 0x10 |
CP2105 - Enhanced Port.
Enhanced port, on Open, Tx
| #define FC_OPEN_TX_IFC0 0x0001 |
CP2108.
CP2108 port 0, on Open, Tx
| #define FC_OPEN_TX_IFC1 0x0010 |
CP2108 port 1, on Open, Tx.
| #define FC_OPEN_TX_IFC2 0x0100 |
CP2108 port 2, on Open, Tx.
| #define FC_OPEN_TX_IFC3 0x1000 |
CP2108 port 3, on Open, Tx.
| #define FC_OPEN_TX_SCI FC_OPEN_TX |
CP2105 - Standard Port.
Standard port, on Open, Tx