Macros | |
| #define | HID_SMBUS_GPIO_FUNCTION 0 |
| GPIO function as configured using direction and mode. More... | |
| #define | HID_SMBUS_SPECIAL_FUNCTION 1 |
| Special function: GPIO.0 - TX Toggle (push - pull output) GPIO.1 - RX Toggle (push - pull output) GPIO.7 - Clock Output (push - pull output) More... | |
| #define HID_SMBUS_GPIO_FUNCTION 0 |
GPIO function as configured using direction and mode.
| #define HID_SMBUS_SPECIAL_FUNCTION 1 |
Special function: GPIO.0 - TX Toggle (push - pull output) GPIO.1 - RX Toggle (push - pull output) GPIO.7 - Clock Output (push - pull output)