Macros | |
| #define | HID_SMBUS_MASK_FUNCTION_GPIO_7_CLK 0x01 |
| Enables or disables the clock output function of GPIO.7. More... | |
| #define | HID_SMBUS_MASK_FUNCTION_GPIO_0_TXT 0x02 |
| Enables or disables the TX toggle function of GPIO.0. More... | |
| #define | HID_SMBUS_MASK_FUNCTION_GPIO_1_RXT 0x04 |
| Enables or disables the RX toggle function of GPIO.1. More... | |
| #define HID_SMBUS_MASK_FUNCTION_GPIO_0_TXT 0x02 |
Enables or disables the TX toggle function of GPIO.0.
| #define HID_SMBUS_MASK_FUNCTION_GPIO_1_RXT 0x04 |
Enables or disables the RX toggle function of GPIO.1.
| #define HID_SMBUS_MASK_FUNCTION_GPIO_7_CLK 0x01 |
Enables or disables the clock output function of GPIO.7.