Silicon Labs Host Libraries
Pin Bitmasks definitions

Macros

#define CP2114_MASK_GPIO_0   0x0001
 CP2114 gpio 0 mask. More...
 
#define CP2114_MASK_GPIO_1   0x0002
 CP2114 gpio 1 mask. More...
 
#define CP2114_MASK_GPIO_2   0x0004
 CP2114 gpio 2 mask. More...
 
#define CP2114_MASK_GPIO_3   0x0008
 CP2114 gpio 3 mask. More...
 
#define CP2114_MASK_GPIO_4   0x0010
 CP2114 gpio 4 mask. More...
 
#define CP2114_MASK_GPIO_5   0x0020
 CP2114 gpio 5 mask. More...
 
#define CP2114_MASK_GPIO_6   0x0040
 CP2114 gpio 6 mask. More...
 
#define CP2114_MASK_GPIO_7   0x0080
 CP2114 gpio 7 mask. More...
 
#define CP2114_MASK_GPIO_8   0x0100
 CP2114 gpio 8 mask. More...
 
#define CP2114_MASK_GPIO_9   0x0200
 CP2114 gpio 9 mask. More...
 
#define CP2114_MASK_TX   0x0400
 CP2114 gpio tx mask. More...
 
#define CP2114_MASK_RX   0x0800
 CP2114 gpio rx mask. More...
 
#define CP2114_MASK_SUSPEND   0x1000
 CP2114 gpio suspend mask. More...
 
#define CP2114_MASK_SUSPEND_BAR   0x2000
 CP2114 gpio suspend bar mask. More...
 

Detailed Description

Pin Bitmasks

Macro Definition Documentation

◆ CP2114_MASK_GPIO_0

#define CP2114_MASK_GPIO_0   0x0001

CP2114 gpio 0 mask.

◆ CP2114_MASK_GPIO_1

#define CP2114_MASK_GPIO_1   0x0002

CP2114 gpio 1 mask.

◆ CP2114_MASK_GPIO_2

#define CP2114_MASK_GPIO_2   0x0004

CP2114 gpio 2 mask.

◆ CP2114_MASK_GPIO_3

#define CP2114_MASK_GPIO_3   0x0008

CP2114 gpio 3 mask.

◆ CP2114_MASK_GPIO_4

#define CP2114_MASK_GPIO_4   0x0010

CP2114 gpio 4 mask.

◆ CP2114_MASK_GPIO_5

#define CP2114_MASK_GPIO_5   0x0020

CP2114 gpio 5 mask.

◆ CP2114_MASK_GPIO_6

#define CP2114_MASK_GPIO_6   0x0040

CP2114 gpio 6 mask.

◆ CP2114_MASK_GPIO_7

#define CP2114_MASK_GPIO_7   0x0080

CP2114 gpio 7 mask.

◆ CP2114_MASK_GPIO_8

#define CP2114_MASK_GPIO_8   0x0100

CP2114 gpio 8 mask.

◆ CP2114_MASK_GPIO_9

#define CP2114_MASK_GPIO_9   0x0200

CP2114 gpio 9 mask.

◆ CP2114_MASK_RX

#define CP2114_MASK_RX   0x0800

CP2114 gpio rx mask.

◆ CP2114_MASK_SUSPEND

#define CP2114_MASK_SUSPEND   0x1000

CP2114 gpio suspend mask.

◆ CP2114_MASK_SUSPEND_BAR

#define CP2114_MASK_SUSPEND_BAR   0x2000

CP2114 gpio suspend bar mask.

◆ CP2114_MASK_TX

#define CP2114_MASK_TX   0x0400

CP2114 gpio tx mask.