Macros | |
| #define | UNREFERENCED_PARAMETER(p) (void)(p) |
| Unreferenced parameter definition. More... | |
| #define | SILABS_TEST_FILL 0xa5 |
| 10100101 A "fill" pattern, typically only used in Debug situations More... | |
| #define | CP210X_PARTNUM SILABS_PARTNUM_CPXXXX |
Typedefs | |
| typedef unsigned char | BYTE |
| Byte definition. More... | |
| typedef enum _SILABS_VID * | PSILABS_VID |
| silabs vid pointer More... | |
| typedef enum _SILABS_PID * | PSILABS_PID |
| silabs pid pointer More... | |
| typedef enum _SILABS_PARTNUM_CPXXXX * | PSILABS_PARTNUM_CPXXXX |
| Device Part Numbers pointer. More... | |
| typedef enum _SILABS_STATUS * | PSILABS_STATUS |
| API Status return codes pointer. More... | |
Enumerations | |
| enum | SILABS_VID { SILABS_VID_10C4 = ((unsigned short)(0xFFFF & 0x10C4)), SILABS_VID_1BA4 = ((unsigned short)(0xFFFF & 0x1BA4)), SILABS_VID_2544 = ((unsigned short)(0xFFFF & 0x2544)) } |
| enum | SILABS_PID { SILABS_PID_UNKNOWN = ((unsigned short)(0xFFFF & 0x0000)), SILABS_PID_CP210SINGLEPORT = ((unsigned short)(0xFFFF & 0xEA60)), SILABS_PID_CP210SINGLEPORTII = ((unsigned short)(0xFFFF & 0xEA63)), SILABS_PID_CP2101 = SILABS_PID_CP210SINGLEPORT, SILABS_PID_CP2102 = SILABS_PID_CP210SINGLEPORT, SILABS_PID_CP2102N = SILABS_PID_CP210SINGLEPORT, SILABS_PID_CP2103 = SILABS_PID_CP210SINGLEPORT, SILABS_PID_CP2104 = SILABS_PID_CP210SINGLEPORT, SILABS_PID_CP210DUALPORT = ((unsigned short)(0xFFFF & 0xEA70)), SILABS_PID_CP210DUALPORTII = ((unsigned short)(0xFFFF & 0xEA7A)), SILABS_PID_CP2105 = SILABS_PID_CP210DUALPORT, SILABS_PID_CP2105II = SILABS_PID_CP210DUALPORTII, SILABS_PID_CP210QUADPORT = ((unsigned short)(0xFFFF & 0xEA71)), SILABS_PID_CP210QUADPORTII = ((unsigned short)(0xFFFF & 0xEA7B)), SILABS_PID_CP2108 = SILABS_PID_CP210QUADPORT, SILABS_PID_CP2108II = SILABS_PID_CP210QUADPORTII, SILABS_PID_CP2109 = SILABS_PID_CP210SINGLEPORT, SILABS_PID_CP2110 = ((unsigned short)(0xFFFF & 0xEA80)), SILABS_PID_CP2111 = SILABS_PID_CP2110, SILABS_PID_CP2112 = ((unsigned short)(0xFFFF & 0xEA90)), SILABS_PID_CP2114 = ((unsigned short)(0xFFFF & 0xEAB0)), SILABS_PID_CP2130 = ((unsigned short)(0xFFFF & 0x87A0)), SILABS_PID_CP2615 = ((unsigned short)(0xFFFF & 0xEAC1)), SILABS_PID_DIRECTACCESS = ((unsigned short)(0xFFFF & 0xEA61)), SILABS_PID_USBXPress = SILABS_PID_DIRECTACCESS } |
| enum | SILABS_PARTNUM_CPXXXX { CP210x_PARTNUM_UNKNOWN = ((BYTE)(0xFF & 0x00)), CP210x_PARTNUM_CP2101 = ((BYTE)(0xFF & 0x01)), CP210x_PARTNUM_CP2102 = ((BYTE)(0xFF & 0x02)), CP210x_PARTNUM_CP2103 = ((BYTE)(0xFF & 0x03)), CP210x_PARTNUM_CP2104 = ((BYTE)(0xFF & 0x04)), CP210x_PARTNUM_CP2105 = ((BYTE)(0xFF & 0x05)), CP210x_PARTNUM_CP2108 = ((BYTE)(0xFF & 0x08)), CP210x_PARTNUM_CP2109 = ((BYTE)(0xFF & 0x09)), SILABS_PARTNUM_CP2110 = ((BYTE)(0xFF & 0x0A)), HID_UART_PART_CP2110 = SILABS_PARTNUM_CP2110, CP210x_PARTNUM_CP2112 = ((BYTE)(0xFF & 0x0C)), HID_SMBUS_PART_CP2112 = CP210x_PARTNUM_CP2112, SILABS_PARTNUM_CP2114 = ((BYTE)(0xFF & 0x0E)), HID_UART_PART_CP2114 = SILABS_PARTNUM_CP2114, CP210x_PARTNUM_CP2102N_QFN28 = ((BYTE)(0xFF & 0x20)), CP210x_PARTNUM_CP2102N_QFN24 = ((BYTE)(0xFF & 0x21)), CP210x_PARTNUM_CP2102N_QFN20 = ((BYTE)(0xFF & 0x22)), CP210x_PARTNUM_USBXPRESS_F3XX = ((BYTE)(0xFF & 0x80)), CP210x_PARTNUM_USBXPRESS_EFM8 = ((BYTE)(0xFF & 0x80)), CP210x_PARTNUM_USBXPRESS_EFM32 = ((BYTE)(0xFF & 0x81)) } |
| enum | SILABS_STATUS { SILABS_STATUS_SUCCESS = ((BYTE)(0xFF & 0x00)), SILABS_STATUS_TBD = ((BYTE)(0xFF & 0x01)), SILABS_STATUS_INVALID_PARAMETER = ((BYTE)(0xFF & 0x02)), SILABS_STATUS_INVALID_HANDLE = ((BYTE)(0xFF & 0x03)), SILABS_STATUS_DEVICE_NOT_FOUND = ((BYTE)(0xFF & 0x04)), SILABS_STATUS_DEVICE_TBD = ((BYTE)(0xFF & 0x05)), SILABS_STATUS_DEVICE_ALREADY_OPENED = ((BYTE)(0xFF & 0x06)), SILABS_STATUS_DEVICE_ERROR = ((BYTE)(0xFF & 0x07)), SILABS_STATUS_DEVICE_ERROR_STATE = ((BYTE)(0xFF & 0x08)), SILABS_STATUS_DEVICE_ERROR_TIMEOUT = ((BYTE)(0xFF & 0x09)), SILABS_STATUS_FUNCTION_NOT_SUPPORTED = ((BYTE)(0xFF & 0x0F)), SILABS_STATUS_MEMORY_ALLOC_ERROR = ((BYTE)(0xFF & 0x44)), SILABS_STATUS_SYSTEM_ERROR = ((BYTE)(0xFF & 0x74)), SILABS_STATUS_UNKNOWN_ERROR = ((BYTE)(0xFF & 0xFF)) } |
Defines common to all Silicon Labs USB Birdge devices (GUIDs, VIDs, PIDs and Part Numbers)
| #define CP210X_PARTNUM SILABS_PARTNUM_CPXXXX |
| #define SILABS_TEST_FILL 0xa5 |
10100101 A "fill" pattern, typically only used in Debug situations
| #define UNREFERENCED_PARAMETER | ( | p | ) | (void)(p) |
Unreferenced parameter definition.
Byte definition.
Device Part Numbers pointer.
silabs pid pointer
API Status return codes pointer.
silabs vid pointer
| enum SILABS_PID |
| Enumerator | |
|---|---|
| SILABS_PID_CP210SINGLEPORT | Single port CP210x device/s. |
| SILABS_PID_CP210SINGLEPORTII | Single port CP210x device/s (Windows Update PID) |
| SILABS_PID_CP2101 | CP2101. |
| SILABS_PID_CP2102 | CP2102. |
| SILABS_PID_CP2102N | CP2102N. |
| SILABS_PID_CP2103 | CP2103. |
| SILABS_PID_CP2104 | CP2104. |
| SILABS_PID_CP210DUALPORT | Dual port CP210x device/s. |
| SILABS_PID_CP210DUALPORTII | Dual port CP210x device/s (Windows Update PID) |
| SILABS_PID_CP2105 | CP2105. |
| SILABS_PID_CP2105II | CP2105 (Windows Update PID) |
| SILABS_PID_CP210QUADPORT | Quad port CP210x device/s. |
| SILABS_PID_CP210QUADPORTII | Quad port CP210x device/s (Windows Update PID) |
| SILABS_PID_CP2108 | CP2108. |
| SILABS_PID_CP2108II | CP2108 (Windows Update PID) |
| SILABS_PID_CP2109 | CP2109. |
| SILABS_PID_CP2110 | CP2110. |
| SILABS_PID_CP2111 | CP2111. |
| SILABS_PID_CP2112 | CP2112. |
| SILABS_PID_CP2114 | CP2114. |
| SILABS_PID_CP2130 | CP2130. |
| SILABS_PID_CP2615 | CP2615. |
| SILABS_PID_DIRECTACCESS | Direct Access. |
| SILABS_PID_USBXPress | Direct Access (nee USBXPress)
|
| enum SILABS_STATUS |
| enum SILABS_VID |