RELEASE NOTES
=============
Silicon Labs USBXpress Host SDK for USB bridge products for Linux

Package version: 6.7.7
Release date:    2022-08-17

This package is the Linux Software Development Kit (SDK) for Silicon Labs
USBXpress and Classic USB bridge products.  It includes support for the
following products:

* CP2102N   (VCP UART)
* CP2102    (VCP UART)
* CP2104    (VCP UART)
* CP2105    (Dual VCP UART)
* CP2108    (Quad VCP UART)
* CP2110    (HID UART)
* CP2112    (HID I2C)
* CP2114    (USB Audio)
* CP2130    (USB SPI)
* CP2615    (USB Audio)

The SDK is intended for application developers using the above Silicon
Labs products.  The SDK provides interface libraries, header files,
documentation and examples.

This package does not contain the VCP driver or Direct Access
Driver (USBXpress driver).  These drivers can be found in their own
installer packages, downloaded from the Silicon Labs web site.

All host software support for Silicon Labs classic and USBXpress USB bridge
devices has been combined into this single Software Development Kit.
This combined SDK package now replaces the individual, per-device installer
packages.

The SDK is organized according to device.  During installation you can
choose to install support for any or all of the devices.  Each device
directory contains the following subdirectories:

* bin - executables.
* include - header files used for compiling programs against the libraries.
* lib - libraries and language bindings.
* Documentation - Data sheets, application notes, user guides and misc.
* python - contains python scripts to test the libraries.
* srcpkg - contains source code of libraries and examples.

For HID devices (cp2112, cp2110 etc ...), they will enter suspend state after
 several seconds when you don't interact with them, 
so you need to go out from suspend state before you running the examples. you can do
 it by sending some commands to them or resetting the boards.

OS VERSIONS
-----------
The binaries were built and tested with Ubuntu 16.04.  They will likely
work with other Linux distributions as well.  Source packages are also
provided so that the binaries can be rebuilt for other systems.

INSTALLING
----------
Uncompress the archive with the following command:
	tar -zxvf USBXpressHostSDK.tar.gz
For installing libraries  in lib folder of modules, go to srcpkg folder of the module, 
then go to folder containing souce code of the lib, then type:
	make
	sudo make install
UNINSTALLING
------------
Delete the folder containing the software. If you have installed a source 
package, you will need to delete the components it has installed. The default
location for these is:
	/usr/local/include
	/usr/local/lib

******************************************************************************
    RELEASE NOTES FOR 6.7.7 (2022-08-17)

Changes for HID SmBus library
==============================================================================
MCUSW-1272   | Improve to add the cp2112smt tool for CP2112                   

Changes for test infrastructure related
==============================================================================
MCUSW-1209   | Add the ComPortTestSuite.py to python package of CP2110_4      
MCUSW-1222   | Fix error  CP210x_GetNumDevices()  in ChangeVIDPID.py test     
             | script.                                                        
MCUSW-1226   | Improve the test script SLABHIDDeviceAPI_Test.py of Cp2110_4 to
             | show test result.                                              

Changes for HID Device library
==============================================================================
MCUSW-1232   | Improve the test script SLABHIDDeviceAPI_Test.py of CP2112 to  
             | show test result                                               

Changes for Host side example code
==============================================================================
MCUSW-1223   | Fix CP210x build error of CP210xsmt Example project            
MCUSW-1233   | Improve to add the CP2130smt application to CP2130 folder      
MCUSW-1235   | Improve to add the makefile to  libusb_example project of      
             | CP2130                                                         
MCUSW-1247   | Fix Zeromemory function error for CP210xsmt/CP2110smt          
MCUSW-1250   | Fix warning for example project in srcpkg folder of CP210x     
MCUSW-1251   | Fix warning for example project in srcpkg folder of CP2110     
MCUSW-1252   | Fix warning for example project in srcpkg folder of CP2112     
MCUSW-1253   | Fix warning for example project in srcpkg folder of CP2130     
MCUSW-1254   | Fix warning for example project in srcpkg folder of CP2615     
MCUSW-1258   | Update SDK layout and add new hidSmbusExample                  
MCUSW-1265   | Fix warning for libusb_example project of CP2130               
MCUSW-1280   | Fix error HidUartExample cannot load .so lib at srcpkg folder  
             | on 32 bit                                                      

Changes for manufacturing and config tools
==============================================================================
MCUSW-1259   | Add path of shared libraries into makefile for smt application 
             | to load .so files.                                             

Changes for HID UART library
==============================================================================
MCUSW-1278   | Update library for customizer tools of CP2110_4                


******************************************************************************
    RELEASE NOTES FOR 6.7.6 (2018-11-12)

Changes for manufacturing and config tools
==============================================================================
MCUSW-94     | Corrects a problem where the VID of the part was being          
             | overwritten when setting other configurable fields.             
MCUSW-114    | Changed the format of the smt-operation guide to PDF.           
MCUSW-115    | Removed unnecessary link commands for libslabhidtouart,         
             | libslabhidtosmbus, libslabhiddevice, and libslab_usb_spi from   
             | the makefile for cp210xsmt.                                     
MCUSW-121    | Mac/Linux smt binaries are now statically linked with Silicon   
             | Labs libraries.                                                 
MCUSW-150    | Resolved an issue whereby CP2615[smt,cfg].exe failed to start   
             | if Microsoft redistributable DLLs were not present on the       
             | machine.                                                        
MCUSW-295    | Fixed an issue where non-programable bits in the QuadPortConfig 
             | field of a CP2108 configuration file corresponding to the state 
             | of the suspend pin were being incorrectly compared during       
             | verification.                                                   
MCUSW-344    | Fixed a problem where the CP2615 utility cp2615smt did not      
             | correctly erase previous configuration when programming a new   
             | configuration.                                                  

Changes for Host side example code
==============================================================================
MCUSW-118    | Added header and library search paths to the libusb_example     
             | xcode project for the CP2130 in order to pick up libusb from    
             | the default location used by homebrew.                          
MCUSW-159    | Added an example program called MacGPIOExample to show how to   
             | use the GPIO pins on the Mac using the 5.x Mac VCP Driver.      
MCUSW-163    | Added the HidUartExample.tar.gz source package to the           
             | CP2110_4/Examples folder.                                       
MCUSW-233    | Added cp2130_libusb_writeread_example(). All example operations 
             | read the TransferPriority byte to determine endpoint            
             | assignments.                                                    

Changes for Installer packages
==============================================================================
MCUSW-116    | Removed data sheets, data shorts, errata and user guide         
             | documents for deprecated VCP parts CP2101 and CP2103.           
MCUSW-117    | Added a QuickStart Guide and a User Guide for the CP2114.       
MCUSW-253    | Add "RCP App" customizer to USBXpress SDK package.              
MCUSW-286    | Add CP2114 customizer to host SDK package.                      
MCUSW-375    | Added HTML API documentation to Docs directory.                 
MCUSW-378    | MacOS - Removed 32 bit code from binaries.                      

Changes for USB SPI library (CP2130)
==============================================================================
MCUSW-15     | Fix USB "direction" bug for CP213x_GetLock() (Windows           
             | SLAB_USB_SPI.DLL CP2130 interface library), which put the       
             | device into a Stall situation and subsequent API calls failed.  
MCUSW-126    | Fix a bug where a file descriptor had not been properly closed  
             | in CP213x_TransferWriteRead.                                    
MCUSW-128    | SLAB_USB_SPI.h is now a single file for Windows, Mac, and       
             | Linux.                                                          

Changes for CP210x Runtime library
==============================================================================
MCUSW-237    | CP210x Runtime library no longer needs/requires to also be      
             | linked to CP210x Manufacturing library, with the newly added    
             | "discovery" APIs CP210xRT_GetNumDevices(), CP210xRT_Open() and  
             | CP210xRT_Close().                                               

Changes for CP210x Manufacturing library
==============================================================================
MCUSW-374    | GetFirmwareVersion() is now supported in the Manufacturing      
             | library for the CP2105 and CP2108.                              

Changes for HID UART library
==============================================================================
MCUSW-180    | Fix device indexing problem for CP2114 devices configured as    
             | OUT-only or IN-only (for which the HID interface is MI_02).     

Changes for SiUSBXp Direct Access Library
==============================================================================
MCUSW-179    | Reduce the timeout for the "Get Part Library version" command   
             | only, called in SI_Open() to 50milliseconds.  This means old    
             | firmware will experience this timeout.                          

Changes for Library language wrappers
==============================================================================
MCUSW-125    | Added the function HidSmbus_CancelIo to the HidtoSMBUS library  
             | on MacOS X.                                                     

Changes for HID SmBus library
==============================================================================
MCUSW-203    | On Linux, libslabhidtosmbus and libslabhidtouart now have a     
             | dependency on libslabhiddevice so that your Linux apps no       
             | longer need to explicitly link to libslabhiddevice.             



******************************************************************************
    RELEASE NOTES FOR 6.7.5 (2017-05-26)

Changes for Installer packages
==============================================================================
MCUSW-8      | SiLabs USBXpress SDK is now available as a debian package.      
MCUSW-86     | CP2615 added to the SDK.                                        
MCUSW-92     | Added a quick start guide and a user guide for the CP2102N to   
             | the SDK package.                                                
MCUSW-99     | This is the first release of our combined host SDK.  All host   
             | software support for Silicon Labs classic and USBXpress USB     
             | bridge devices has been combined into this single Software      
             | Development Kit.  This combined SDK package now replaces the    
             | individual, per-device installer packages.                      

Changes for Host side example code
==============================================================================
MCUSW-9      | The HidUartExample is now available for MacOS X.                
MCUSW-10     | hidUARTExample now available for Linux.                         
MCUSW-11     | The libusb example is now available for Mac and Linux in the    
             | CP2130 package.                                                 

Changes for CP210x Manufacturing library
==============================================================================
MCUSW-76     | Fixed a bug in manufacturing library                            
             | CP210x_GetDeviceInterfaceString() function which presented on   
             | being called for CP2105/CP2108 devices configured with the      
             | USBXpress PID 0xEA61.                                           
MCUSW-96     | CP210xManufacturingDLL.h has been fully SAL-annotated           
             | (https://docs.microsoft.com/en-us/visualstudio/code-            
             | quality/using-sal-annotations-to-reduce-c-cpp-code-defects).    

Changes for CP210x Runtime library
==============================================================================
MCUSW-95     | CP210xRuntimeDLL.h has been fully SAL-annotated                 
             | (https://docs.microsoft.com/en-us/visualstudio/code-            
             | quality/using-sal-annotations-to-reduce-c-cpp-code-defects).    

Changes for manufacturing and config tools
==============================================================================
MCUSW-13     | Fixed a bug that prevented the programming of serial numbers on 
             | the CP2102N using the cp210xsmt utility.