The AWS SDK for Java enables Java developers to easily work with Amazon Web Services and build scalable solutions with Amazon S3, Amazon DynamoDB, Amazon Glacier, and more. You can get started in minutes using Maven or by downloading a single zip file.
Before you begin, you need an AWS account. Please see the Sign Up for AWS section of the developer guide for information about how to create an AWS account and retrieve your AWS credentials.
To run the SDK you will need Java 1.6+. For more information about the requirements and optimum settings for the SDK, please see the Installing a Java Development Environment section of the developer guide.
The recommended way to use the AWS SDK for Java in your project is to consume it from Maven. Import the aws-java-sdk-bom and specify the SDK Maven modules that your project needs in the dependencies.
xml
<dependencyManagement>
<dependencies>
<dependency>
<groupId>com.amazonaws</groupId>
<artifactId>aws-java-sdk-bom</artifactId>
<version>1.11.52</version>
<type>pom</type>
<scope>import</scope>
</dependency>
</dependencies>
</dependencyManagement>
xml
<dependencies>
<dependency>
<groupId>com.amazonaws</groupId>
<artifactId>aws-java-sdk-ec2</artifactId>
</dependency>
<dependency>
<groupId>com.amazonaws</groupId>
<artifactId>aws-java-sdk-s3</artifactId>
</dependency>
<dependency>
<groupId>com.amazonaws</groupId>
<artifactId>aws-java-sdk-dynamodb</artifactId>
</dependency>
</dependencies>
See the Set up the AWS SDK for Java section of the developer guide for more information about installing the SDK through other means.
Provides easy-to-use HTTP clients for all supported AWS services, regions, and authentication protocols.
Client-Side Data Encryption for Amazon S3 - Helps improve the security of storing application data in Amazon S3.
Amazon DynamoDB Object Mapper - Uses Plain Old Java Object (POJOs) to store and retrieve Amazon DynamoDB data.
Amazon S3 Transfer Manager - With a simple API, achieve enhanced the throughput, performance, and reliability by using multi-threaded Amazon S3 multipart calls.
Amazon SQS Client-Side Buffering - Collect and send SQS requests in asynchronous batches, improving application and network performance.
Automatically uses IAM Instance Profile Credentials on configured Amazon EC2 instances.
And more!
Once you check out the code from GitHub, you can build it using Maven. To disable the GPG-signing in the build, use:
sh
mvn clean install -Dgpg.skip=true
1.11.x - Recommended.
1.10.x - Approved. Only major critical bugs will be fixed. To get the new features, upgrade to 1.11.x version of the SDK.