How to Unfollow Your Email Subscriptions 

On the community, you can choose to follow an individual thread or/and a forum board which is consists of multiple threads. If you still receive email notifications from the Silicon Labs Community after turning your email settings off, you may need to Unfollow the thread or the forum board that you are following directly. 
 

Please follow these steps:

1. Open your email from the Silicon Labs Community.
2. Click the ‘Click this link’ text under the community content to see where the email update came from. 

3. Select Unfollow All, if you land on the thread page that you are following.  

4. If you are not following any thread, check its forum board. You may have followed an entire forum instead of a thread if you received multiple email notifications from the same forum board.

 

The list of forum boards:

8-bit MCUs

32-bit MCUs

Bluetooth

ZigBee and Thread

Proprietary

Z-Wave

Wi-Fi

Interface

Sensors

Isolation

Timing

Power

Simplicity Studio

Thunderboard

 

5. Select Unfollow All, if you followed any forum board. 

6. Please wait and see if you still receive email updates from the community. If it still doesn’t work, please contact DL.Feedback@silabs.com for further assistance.