Silicon Labs
|
Silicon Labs Community Silicon Labs Community
  • Products
    1. 8-bit MCU
    2. 32-bit MCU
    3. Bluetooth
    4. Proprietary
    5. Wi-Fi
    6. Zigbee & Thread
    7. Z-Wave
    8. Interface
    9. Isolation
    10. Power
    11. Sensors
    12. Timing
  • Development Tools
    1. Simplicity Studio
    2. Third Party Tools
  • Expert's Corner
    1. Announcements
    2. Blog
    3. General Interest
    4. Projects
How to Buy
English
  • English
  • 简体中文
  • 日本語
//
Community // Blog

Speed Does Not Kill: Power Supplies with Fast Switching Frequency Get Safer

05/136/2017 | 02:00 PM
Lance Looper
Employee

Level 5


The more power generated by a smaller power supply, the more cost effective it is and the less room it takes in the design. Designers can improve W/mm3 with faster switching. Switching technology using Gallium Nitride (GaN) or Silicon Carbide (SiC) allows faster switching rates than are currently available—up to 20 times faster.

 

The technologies’ lateral structures, compared to vertical for silicon, make them low-charge devices capable of switching hundreds of volts in mere nano-seconds (ns). The challenge is that they require isolated gate drivers to work, and today’s technology typically cannot support the required noise immunity from their superfast switching.

 

Faster Switching - SMPS Want It

Fast power switching is most prevalent in switched mode power supplies (SMPS). SMPS convert their input power from ac to dc (ac-dc) or from dc to dc (dc-dc). In most cases, they also change voltage levels to suit the needs of the application.

 

SMPS Graphic.png

Typical ac-dc SMPS block diagram

 

The new GaN and SiC technology switches faster and is more efficient than current switches. But their faster switching causes higher switching transients as shown in the figure below with a typical 600 V high side rail.

Switching Transients.png

Switching transients in a power converter

 

GaN switching times are typically about 5ns, or about 10x - 20x faster than conventional systems. In this case, the 600 V high voltage rail results in a 120 kV/µs transient (600 V / 5 ns = 120 V/ns or 120 kV/µs).

 

CMTI – Common Mode Transient Immunity – the Key Isolated Gate Driver Spec

The isolated gate drivers controlling the power switches have to be designed to withstand these noise transients without creating glitches or latching-up. The ability of the driver to withstand these common mode noise transients is generally defined as CMTI (common mode transient immunity), and is expressed in units of kV/µs.

 

 

What are the Isolated Gate Driver Options?

Isolated gate drivers must preserve the integrity of the isolation from the primary to the secondary side. There are a number of isolated gate driver solutions available today:

 

  • Junction-isolated drivers – With 50 kV/µs for latch-up immunity (CMTI proxy), these are not suitable for new, fast-switching tech’s requirement.
  • Opto-coupled drivers – With 10-50 kV/µs for latch-up immunity (CMTI proxy), these are still not good enough.
  • Transformer-coupled drivers – Getting closer with 50-100 kV/µs for latch-up immunity (CMTI proxy), but these are still not adequate.
  • Capacitive-coupled drivers – She’s got it where it counts. These explicitly specify CMTI at 200 kV/µs (MIN) for signal integrity and 400 kV/µs (MAX) for latch-up immunity. These exceed the 120 kV/µs requirement.

 

There are other advantages for these drivers. Their latency (propagation delay) can be as much as 10x better than popular optocoupled gate drivers, and their part-to-part matching can be more than 10x better. This provides the designer with another key advantage—the system’s overall modulation scheme can be fine-tuned for maximum efficiency (W/mm3) and safety without having to accommodate specification slop. They also support lower voltage operation (2.5 V compared to 5 V) and a wider operating temperature range.

 

Plus, they offer advanced features such as input noise filters, asynchronous shutdown capability, and multiple configurations such as half bridge or dual independent drivers in a single package.

Finally, they are rated to 60 years of operating life at high voltage conditions, longer than any other comparable solution.

 

Power supply designers want to maximize their W/mm3 using the fastest power switching technology available. The latest GaN- and SiC-based switches are the fastest available technology today, but isolated require gate drivers with very high noise immunity (CMTI).

 

The Si827x isolated gate drivers from Silicon Labs meet GaN’s and SiC’s noise immunity requirements with margin to spare (120 kV/µs required, 200 kV/µs supplied).

 

Si827x.png

  • Blog Posts
  • Internet Infrastructure
  • Timing

Tags

  • Wireless
  • High Performance Jitter Attenuators
  • EFR32FG22 Series 2 SoCs
  • EFR32MG21 Series 2 SoCs
  • Security
  • Bluegiga Legacy Modules
  • Zigbee SDK
  • ZigBee and Thread
  • EFR32BG13 Series 1 Modules
  • Internet Infrastructure
  • Sensors
  • Wireless Xpress BGX13
  • Blue Gecko Bluetooth Low Energy SoCs
  • Z-Wave
  • Micrium OS
  • Blog Posts
  • Low Jitter Clock Generators
  • Bluetooth Classic
  • Makers
  • Flex SDK
  • Tips and Tricks
  • timing
  • Smart Cities
  • Smart Homes
  • IoT Heroes
  • Reviews
  • RAIL
  • Simplicity Studio
  • Tiny Gecko
  • EFR32MG22 Series 2 SoCs
  • Mighty Gecko SoCs
  • Timing
  • Temperature Sensors
  • Blue Gecko Bluetooth Low Energy Modules
  • Ultra Low Jitter Clock Generators
  • General Purpose Clock Generators
  • EFR32BG22 Series 2 SoCs
  • Industry 4.0
  • Giant Gecko
  • 32-bit MCUs
  • Bluetooth Low Energy
  • 32-bit MCU SDK
  • Gecko
  • Microcontrollers
  • Jitter Attenuators
  • EFR32BG21 Series 2 SoCs
  • News and Events
  • Industrial Automation
  • Wi-Fi
  • Bluetooth SDK
  • Community Spotlight
  • Clock Generators
  • Biometric Sensors
  • General Purpose Jitter Attenuators
  • Giant Gecko S1
  • WF200
  • Flex Gecko
  • Internet of Things
  • 8-bit MCUs
  • Wireless Jitter Attenuators
  • Isolation
  • Powered Devices
  • Power

Top Authors

  • Avatar image Siliconlabs
  • Avatar image Jackie Padgett
  • Avatar image Nari Shin
  • Avatar image lynchtron
  • Avatar image deirdrewalsh
  • Avatar image Lance Looper
  • Avatar image lethawicker

Archives

  • 2016 January
  • 2016 February
  • 2016 March
  • 2016 April
  • 2016 May
  • 2016 June
  • 2016 July
  • 2016 August
  • 2016 September
  • 2016 October
  • 2016 November
  • 2016 December
  • 2017 January
  • 2017 February
  • 2017 March
  • 2017 April
  • 2017 May
  • 2017 June
  • 2017 July
  • 2017 August
  • 2017 September
  • 2017 October
  • 2017 November
  • 2017 December
  • 2018 January
  • 2018 February
  • 2018 March
  • 2018 April
  • 2018 May
  • 2018 June
  • 2018 July
  • 2018 August
  • 2018 September
  • 2018 October
  • 2018 November
  • 2018 December
  • 2019 January
  • 2019 February
  • 2019 March
  • 2019 April
  • 2019 May
  • 2019 June
  • 2019 July
  • 2019 August
  • 2019 September
  • 2019 October
  • 2019 November
  • 2019 December
  • 2020 January
  • 2020 February
  • 2020 March
  • 2020 April
  • 2020 May
  • 2020 June
  • 2020 July
  • 2020 August
  • 2020 September
  • 2020 October
  • 2020 November
  • 2020 December
  • 2021 January
Silicon Labs
Stay Connected With Us
Plug into the latest on Silicon Labs products, including product releases and resources, documentation updates, PCN notifications, upcoming events, and more.
  • About Us
  • Careers
  • Community
  • Contact Us
  • Corporate Responsibility
  • Privacy and Terms
  • Press Room
  • Investor Relations
  • Site Feedback
  • Cookies
Copyright © Silicon Laboratories. All rights reserved.
粤ICP备15107361号
Also of Interest:
  • Bring Your IoT Designs to Life with Smart,...
  • IoT Hero CoreTigo Drives New Wireless Standard...
  • A Guide to IoT Protocols at Works With...