Silicon Labs
|
Silicon Labs Community Silicon Labs Community
  • Products
    1. 8-bit MCU
    2. 32-bit MCU
    3. Bluetooth
    4. Proprietary
    5. Wi-Fi
    6. Zigbee & Thread
    7. Z-Wave
    8. Interface
    9. Isolation
    10. Power
    11. Sensors
    12. Timing
  • Development Tools
    1. Simplicity Studio
    2. Third Party Tools
  • Expert's Corner
    1. Announcements
    2. Blog
    3. General Interest
    4. Projects
How to Buy
English
  • English
  • 简体中文
  • 日本語
//
Community // Blog

Solving Wi-Fi Power Consumption Issues in IoT Applications

02/43/2019 | 07:58 PM
Lance Looper
Employee

Level 5


There is a huge demand today for adding Wi-Fi connectivity to IoT applications because of the many advantages over other wireless protocols (Zigbee, Bluetooth, etc.) such as longer range, native IP connectivity, and high bandwidth. For millions of IoT applications, including industrial machines and sensors, Wi-Fi is often the best choice for connectivity because of its robust infrastructure and global reach- Wi-Fi exists almost everywhere in the world today.

 

Challenges for developers: The biggest challenge for developers has been the high-power consumption of Wi-Fi in IoT systems. Wi-Fi protocols were designed primarily to optimize bandwidth, range, and throughput, not power consumption. This makes it a poor choice for power-constrained applications that rely on battery power. Of the various cons of using standard Wi-Fi protocols, high power consumption is the most impactful (range limitations and busy networks are cons as well). Until today, developers have avoided adding Wi-Fi to their IoT applications as there hasn’t been a viable option for adding Wi-Fi connectivity to battery operated devices that didn’t require high power consumption.

These are the four key challenges when adding Wi-Fi connectivity:

  • selecting the appropriate Wi-Fi protocol for energy efficiency
  • costly compared to other protocols
  • more time and resources needed compared to other wireless protocols
  • form factor constraints

Power consumption in Wi-Fi varies dramatically across various modes of operation and it’s important to understand the different modes and optimize them to reduce overall power consumption. One strategy is to stay in the lowest power mode as much as possible and transmit/receive data quickly when needed.

 

RF performance: Unlike many wireless protocols, Wi-Fi power consumption is significantly impacted by RF performance and network conditions. This is a significant problem with the increasingly crowded Wi-Fi networks today. A busy network leads to many retries/retransmissions which consumes a high level of power. Developers must focus on reducing retransmissions and controlling link budgets to be successful.

Wi-Fi devices typically consume significant power in both Transmit (Tx) and Receive (Rx) modes. There are several ways to reduce power consumption and optimize Tx and Rx modes. First choose devices with high selectivity/out of band rejection. Also, choose devices with high Rx sensitivity, and if possible, choose uncrowded channels for device operation. This might mean using channels not used by chatty connections such as video streaming.

 

Applications: Power consumption is highly dependent on the application and use case. IoT applications typically fall into one of three categories:

Always on/connected-these devices are always on which allows users to access the device remotely at any time via cloud or mobile application.  A Wi-Fi video camera is a good example of this use case. Latency is a critical factor in these applications and power consumption is dominated by the transmit power mode (the highest power consumption), as the device is transmitting data and it would be detrimental to be inactive or inaccessible.

 

Periodically connected - These devices are connected to a remote server or cloud platform and only need to transmit occasionally. A good example is a temperature or humidity sensor that sends data every few minutes and it can tolerate the small amount of time it takes to become active. Latency is not a major concern and the power consumption is dominated by receive and sleep currents. It stays in intermediate power levels so it’s never completely awake or asleep so it wakes up faster.

 

Event-driven - An online shopping order button is a good example of event-driven Wi-Fi connectivity. It’s almost always inactive/asleep, meaning there is no data transmission. It wakes up infrequently, and it takes longer to wake up from this mode. An event occurs that triggers wakeup such as when a user selects the order button. This mode is dominated by the lowest sleep current and is best when needing to use the least amount of power possible for an IoT application.

 

Design issues -  Lowering Wi-Fi power consumption is also a design system issue and is a critical challenge for developers today. Power management and extended battery life are major factors when developing IoT applications. Although standard Wi-Fi protocols weren’t designed initially for low power operations, there are many techniques to help significantly reduce power consumption. These techniques include optimizing Rx and Tx modes, optimizing power-saving modes (sleep modes, WMM, DTIM, shutdown/standby), choosing the right hardware, using built-in specifications, optimizing RF performance, and system level optimization. Developers must understand all the contributing factors to overall energy consumption in IoT devices.

They must also understand both system-level factors and deep application factors in order to achieve low energy consumption in their applications. Finding the right mix of power-saving Wi-Fi modes and selecting the right hardware are the keys to dramatically reducing power consumption. Leveraging hardware and software designed specifically for IoT devices and low power consumption can reduce long term costs, overcome development challenges, extend battery life, and potentially enhance the life of products and customer satisfaction.

 

We solve the power management issues for IoT developers by providing drop-in Wi-Fi solutions, including pre-programmed modules (WF200 and WGM160) that can cut power consumption in half. These solutions are designed proactively with low power IoT applications in mind and work in a wide range of applications from home automation to commercial, retail, security, and consumer health-care products. Pre-programmed modules provide a prototype quickly which helps developers get products to market faster.

 

To read the full whitepaper on this topic. click here:

 

 

  • Blog Posts
  • Smart Homes
  • Internet of Things
  • Wi-Fi

Tags

  • Wireless
  • High Performance Jitter Attenuators
  • EFR32FG22 Series 2 SoCs
  • EFR32MG21 Series 2 SoCs
  • Security
  • Bluegiga Legacy Modules
  • Zigbee SDK
  • ZigBee and Thread
  • EFR32BG13 Series 1 Modules
  • Internet Infrastructure
  • Sensors
  • Wireless Xpress BGX13
  • Blue Gecko Bluetooth Low Energy SoCs
  • Z-Wave
  • Micrium OS
  • Blog Posts
  • Low Jitter Clock Generators
  • Bluetooth Classic
  • Makers
  • Flex SDK
  • Tips and Tricks
  • timing
  • Smart Cities
  • Smart Homes
  • IoT Heroes
  • Reviews
  • RAIL
  • Simplicity Studio
  • Tiny Gecko
  • EFR32MG22 Series 2 SoCs
  • Mighty Gecko SoCs
  • Timing
  • Temperature Sensors
  • Blue Gecko Bluetooth Low Energy Modules
  • Ultra Low Jitter Clock Generators
  • General Purpose Clock Generators
  • EFR32BG22 Series 2 SoCs
  • Industry 4.0
  • Giant Gecko
  • 32-bit MCUs
  • Bluetooth Low Energy
  • 32-bit MCU SDK
  • Gecko
  • Microcontrollers
  • Jitter Attenuators
  • EFR32BG21 Series 2 SoCs
  • News and Events
  • Industrial Automation
  • Wi-Fi
  • Bluetooth SDK
  • Community Spotlight
  • Clock Generators
  • Biometric Sensors
  • General Purpose Jitter Attenuators
  • Giant Gecko S1
  • WF200
  • Flex Gecko
  • Internet of Things
  • 8-bit MCUs
  • Wireless Jitter Attenuators
  • Isolation
  • Powered Devices
  • Power

Top Authors

  • Avatar image Siliconlabs
  • Avatar image Jackie Padgett
  • Avatar image Nari Shin
  • Avatar image lynchtron
  • Avatar image deirdrewalsh
  • Avatar image Lance Looper
  • Avatar image lethawicker

Archives

  • 2016 January
  • 2016 February
  • 2016 March
  • 2016 April
  • 2016 May
  • 2016 June
  • 2016 July
  • 2016 August
  • 2016 September
  • 2016 October
  • 2016 November
  • 2016 December
  • 2017 January
  • 2017 February
  • 2017 March
  • 2017 April
  • 2017 May
  • 2017 June
  • 2017 July
  • 2017 August
  • 2017 September
  • 2017 October
  • 2017 November
  • 2017 December
  • 2018 January
  • 2018 February
  • 2018 March
  • 2018 April
  • 2018 May
  • 2018 June
  • 2018 July
  • 2018 August
  • 2018 September
  • 2018 October
  • 2018 November
  • 2018 December
  • 2019 January
  • 2019 February
  • 2019 March
  • 2019 April
  • 2019 May
  • 2019 June
  • 2019 July
  • 2019 August
  • 2019 September
  • 2019 October
  • 2019 November
  • 2019 December
  • 2020 January
  • 2020 February
  • 2020 March
  • 2020 April
  • 2020 May
  • 2020 June
  • 2020 July
  • 2020 August
  • 2020 September
  • 2020 October
  • 2020 November
  • 2020 December
  • 2021 January
Silicon Labs
Stay Connected With Us
Plug into the latest on Silicon Labs products, including product releases and resources, documentation updates, PCN notifications, upcoming events, and more.
  • About Us
  • Careers
  • Community
  • Contact Us
  • Corporate Responsibility
  • Privacy and Terms
  • Press Room
  • Investor Relations
  • Site Feedback
  • Cookies
Copyright © Silicon Laboratories. All rights reserved.
粤ICP备15107361号
Also of Interest:
  • Bring Your IoT Designs to Life with Smart,...
  • IoT Hero CoreTigo Drives New Wireless Standard...
  • A Guide to IoT Protocols at Works With...