Silicon Labs
|
Silicon Labs Community Silicon Labs Community
  • Products
    1. 8-bit MCU
    2. 32-bit MCU
    3. Bluetooth
    4. Proprietary
    5. Wi-Fi
    6. Zigbee & Thread
    7. Z-Wave
    8. Interface
    9. Isolation
    10. Power
    11. Sensors
    12. Timing
  • Development Tools
    1. Simplicity Studio
    2. Third Party Tools
  • Expert's Corner
    1. Announcements
    2. Blog
    3. General Interest
    4. Projects
How to Buy
English
  • English
  • 简体中文
  • 日本語
//
Community // Blog

Kernel 201: Task Architecture & Communication

06/165/2019 | 09:11 PM
Mark Mulrooney
Employee

Level 5


This blog is part of the Kernel 201: Designing a Dynamic Multiprotocol Application with Micrium OS. The table of contents for this blog series can be found here.

Note: It is recommended to download the Kernel 201 application and have the code in front of you as you go through this blog post. The code can be downloaded on the Kernel 201: Project Resources page. 

Task Architecture

The first step of designing any real-time system, before writing any code, is to identify all events the system will be responsible for. Listing out these actions will help identify what events may be grouped together in tasks and what actions will require their own task/s. There are a number of resources available that discuss different task modeling strategies. Some common strategies you may come across are:

  • Signal event groups – Every event is put in its own task. Not efficient in large systems.
  • Sequential events – Events that must be processed in order can be grouped together.
  • Timing events – Events that occur on a periodic time base can be grouped together
  • Interface events – All events associated with a particular interface
  • Safety monitoring – Any safety monitoring events should be separated from any actuation tasks

For this application, these are the following events that must be handled and how they’ll be grouped into tasks:

  • Bluetooth TX – labBluetoothTask
  • Bluetooth RX – labBluetoothTask
  • Proprietary Wireless TX – labPropTask
  • Proprietary Wireless RX – labPropTask
  • GPIO LED Control – labLEDTask
  • RBG LED Control – labLEDTask
  • Button 0 Read – labBtnTask
  • Button 1 Read – labBtnTask
  • Hardware Watchdog – labWDOGTask

labBluetoothTask
Silicon Labs’ Bluetooth stack already creates two tasks, Bluetooth and LinkLayer to handle the transmission and reception. The Bluetooth task provides callbacks for the user to implement to know when there is an event to process. The labBluetoothTask will handle those events from the Bluetooth task and pass that data along to the other tasks in the system. The labBluetoothTask will also receive data from other tasks in the system to transmit via Bluetooth.

labPropTask
Silicon Labs does not provide internal tasks for Proprietary Wireless (RAIL) as it does for Bluetooth, but it is important to group the RAIL functions together as they are not thread-safe functions. The labPropTask will handle all data received by RAIL and send it to other tasks in the system as needed. It will also receive data from other tasks in the system and send it out via RAIL.

labLEDTask
Since only the GPIO or RGB LEDs can be active at one time, it makes sense to group them together.

labBtnTask
The button task operates on a low priority polling interval. It could be switched to an interrupt based task but by leaving it as a polling task, it leaves open the option to add other polling events to the task in the future.

labWDOGTask
The watchdog task will implement a software based watchdog to control how the system feeds the hardware watchdog. It is important that this task have no other operations than handling the watchdog.

 

Task Communication

Now that the events have been divided up into their respective tasks, it is important to implement a consistent method for communication between tasks. There are again many different ways to implement task communication. Micrium OS Kernel provides Semaphores, Task Semaphores, Event Flags, Message Queues and Task Message Queues. While each of these kernel objects have various pros and cons, no one of these services is better than another; it just depends on the application and how it is using these kernel services.

For this application, each task (with the exception of the watchdog task) will be centered around a Task Message Queue and the entire application will use a sort-of layered messaging scheme, similar to the OSI model but much more simplified. The main loop of each task will pend on a Task Message Queue and wait for a message or timeout to determine its next action.

The image above shows the basic layout for all tasks in the system. The code snippet below shows some pseudocode for the task

void* p_msg;
LAB_Q_ID_e lab_q_id;

while (DEF_TRUE)
{
    p_msg = OSTaskQPend( LAB_WDOG_TASK_TIMEOUT_MS,     // Block the task until we
                         OS_OPT_PEND_BLOCKING,         //  receive a message
                        &lab_q_id,
                         0,
                        &err);
    do {
        if(err.Code == RTOS_ERR_TIMEOUT) {             // If we timeout, just feed
            break;                                     //  the watchdog task
        } else if(err.Code != RTOS_ERR_NONE) {         // Shouldn't occur, assert
            APP_RTOS_ASSERT_CRITICAL(err.Code == RTOS_ERR_NONE, ;);
        }

        switch(lab_q_id) {
            case LAB_Q_ID_XXX_EVT:
                labXXXHandleEvt();                    // Handle a task event
                break;

            case LAB_Q_ID_MSG:
                labXXXHandleMsg((LAB_MSG_s*) p_msg);  // Handle a lab message
                labUtilMsgFree(p_msg);                // Then free the message
                break;                                //  back to the pool

            default:
                break;
        }
    } while(0);

    labWDOGFeed(LAB_TASK_ID_XXX);                     // Feed the watchdog after 
}                                                     //  every task action

 

By using the Task Message Queue, it allows a task to wait on three different types of events:

  • Timeouts
  • Events
  • Lab Messages

Timeouts

The software watchdog wants every task to check in on a specified rate to show it has not gone out to lunch. By specifying a timeout value in the Task Message Queue pend, the pend call will return with RTOS_ERR_TIMEOUT if a message is not received in the specified time. If a task expects a message in a set time interval, logic can also be added to the error check for RTOS_ERR_TIMEOUT to keep track of how many timeouts we receive in a row.

Events

Some tasks may have a hardware interrupt or software timer callback they need to handle in addition to processing messages from other tasks in the system. The msg_size data field in OSTaskQPend() provides a 32-bit value that is used as an identifier field for this task design. When a task receives a message, it will have a switch statement to handle the value of msg_size. In this application, all message identifiers can be found in an enum called LAB_Q_ID_e.

When an interrupt or software timer callback wants to send a message to the task it is associated with, it will make a call similar to the one below:

OSTaskQPost(&labXXXTaskTCB,
             0,
             LAB_Q_ID_XXX_EVT,
             OS_OPT_POST_FIFO,
            &err);

 

It is important to note that the LAB_Q_ID_e value is specified in the msg_size field and not the void* field. All messages sent must have a valid identifier in the msg_size field where the void* argument is optional. In this case, the void* argument is set to 0 as there is no extra data to send.

Lab Messages

These messages are how tasks communicate with each other in this application. Rather than having the Bluetooth or Proprietary Wireless tasks spend time configuring PWM timers to drive the RGB LEDs, it makes more sense to send the LED task a LED command to be processed. This also allows us to handle wireless communication at a higher priority than changing the LEDs or polling the button states. The wireless tasks may be affected if responses are not sent out at specific intervals where if the system has to wait an extra 10ms to toggle the LED, the user most likely won’t notice.

The lab messages follow a layered model where every message has the same header, the header defines what else is to follow in the packet. This application provides utility functions for getting, sending and freeing messages (refer to lab_util.c). There are advantages to these utility functions that will be discussed a little later. When you get/free a message you are actually pulling from a memory pool of fixed block sizes. All messages, regardless of how much of the block they use, are the same size. In the case of this application, all messages are 32 bytes in size. This means that if a task needs to send or receive a message larger than 32 bytes, either the size of every block in the system must be increased, multiple messages must be sent or modifications must be made to the utility functions to allow for allocation and freeing of different size blocks.

typedef struct {
    LAB_MSG_ID_e id;
    LAB_MSG_TYPE_e type;
    void *p_data;
} LAB_MSG_s;

The struct above shows the lab message structure that all messages will start with. The ID field identifies what message will follow it and the type corresponds to if it’s a command, response, update or error message. The void* argument is used so you can cast the next layer to the end of the lab message struct.

LAB_MSG_s *p_msg;

p_msg = (LAB_MSG_s*) labUtilMsgGet();       // Get a data buffer to send a message
if(p_msg == DEF_NULL) {
    break;
}

p_msg->id = LAB_MSG_ID_LED;                 // Set the message id
p_msg->type = LAB_MSG_TYPE_CMD;             // Set that its a command message

When you wish to allocate a message to send, the code snippet above shows how you would use the labUtil function to allocate a message. The image below shows how the lab message fits into the allocated block.

After you configure the message ID and message type fields, you need to configure the next part of the block for the message ID you specified. For this example, let’s assume we’re changing the LEDs. LEDs are controlled by the LAB_LED_MSG_s struct. To accomplish this, you will cast the LAB_LED_MSG_s to p_data so when you enter information for the LED message, it goes into the correct location in lab message.

LAB_MSG_s *p_msg;
LAB_LED_MSG_s *p_led_msg;

p_msg = (LAB_MSG_s*) labUtilMsgGet();       // Get a data buffer to send a message
if(p_msg == DEF_NULL) {
    break;
}

p_msg->id = LAB_MSG_ID_LED;                 // Set the message id
p_msg->type = LAB_MSG_TYPE_CMD;             // Set that its a command message

p_led_msg = (LAB_MSG_LED_s*) &(p_msg->p_data);

p_led_msg->mode  = LAB_LED_MODE_RGB;
p_led_msg->color = LAB_LED_COLOR_GREEN;
p_led_msg->state = LAB_LED_STATE_BLINK;

The code snippet above shows how to cast the p_data argument to the LED message structure. Now when you modify the fields of the LED message structure it will be aligned in the message block as shown below.

Once the full message is assembled, the message needs to be sent to the desired task/s. Some messages may only go to one task where others may need to be sent to multiple tasks. The lab utility function for sending offers flexibility for sending messages. Using the labUtilSend() function as shown below, you pass the pointer to the message block just configured and the task/s the message should be sent to. 

labUtilMsgSend(p_msg, dest_task);  // Send the message to the specified destination

In the case where one message is being sent to multiple tasks, the send function will keep track of the number of tasks it was sent to. This allows each task to call the free function after its processed the message, but the memory block is not actually freed until all tasks that received the message free it. To free a message all a task needs to do is make the following call:

labUtilMsgFree(p_msg);   // Free the message back to the pool

It is the labUtilMsgFree function's job to determine when the message is actually returned to the message pool. If one task never calls free on the message it received, that block will never be freed and that memory will be lost so it is imperative that all tasks free all messages they receive, even if they receive the message in error. 

Final Thoughts

This wraps up the Task Communication and Architecture section of the Kernel 201 application. Moving forward the Bluetooth, Proprietary Wireless, LED and Button tasks will all be using this communication structure. If you have any questions about this post feel free to leave comments below.

  • Blog Posts
  • Micrium OS

Tags

  • Wireless
  • High Performance Jitter Attenuators
  • EFR32FG22 Series 2 SoCs
  • EFR32MG21 Series 2 SoCs
  • Security
  • Bluegiga Legacy Modules
  • Zigbee SDK
  • ZigBee and Thread
  • EFR32BG13 Series 1 Modules
  • Internet Infrastructure
  • Sensors
  • Wireless Xpress BGX13
  • Blue Gecko Bluetooth Low Energy SoCs
  • Z-Wave
  • Micrium OS
  • Blog Posts
  • Low Jitter Clock Generators
  • Bluetooth Classic
  • Makers
  • Flex SDK
  • Tips and Tricks
  • timing
  • Smart Cities
  • Smart Homes
  • IoT Heroes
  • Reviews
  • RAIL
  • Simplicity Studio
  • Tiny Gecko
  • EFR32MG22 Series 2 SoCs
  • Mighty Gecko SoCs
  • Timing
  • Temperature Sensors
  • Blue Gecko Bluetooth Low Energy Modules
  • Ultra Low Jitter Clock Generators
  • General Purpose Clock Generators
  • EFR32BG22 Series 2 SoCs
  • Industry 4.0
  • Giant Gecko
  • 32-bit MCUs
  • Bluetooth Low Energy
  • 32-bit MCU SDK
  • Gecko
  • Microcontrollers
  • Jitter Attenuators
  • EFR32BG21 Series 2 SoCs
  • News and Events
  • Wi-Fi
  • Bluetooth SDK
  • Community Spotlight
  • Clock Generators
  • Biometric Sensors
  • General Purpose Jitter Attenuators
  • Giant Gecko S1
  • WF200
  • Flex Gecko
  • Internet of Things
  • 8-bit MCUs
  • Wireless Jitter Attenuators
  • Isolation
  • Powered Devices
  • Power

Top Authors

  • Avatar image Siliconlabs
  • Avatar image Jackie Padgett
  • Avatar image Nari Shin
  • Avatar image lynchtron
  • Avatar image deirdrewalsh
  • Avatar image Lance Looper
  • Avatar image lethawicker

Archives

  • 2016 March
  • 2016 April
  • 2016 May
  • 2016 June
  • 2016 July
  • 2016 August
  • 2016 September
  • 2016 October
  • 2016 November
  • 2016 December
  • 2017 January
  • 2017 February
  • 2017 March
  • 2017 April
  • 2017 May
  • 2017 June
  • 2017 July
  • 2017 August
  • 2017 September
  • 2017 October
  • 2017 November
  • 2017 December
  • 2018 January
  • 2018 February
  • 2018 March
  • 2018 April
  • 2018 May
  • 2018 June
  • 2018 July
  • 2018 August
  • 2018 September
  • 2018 October
  • 2018 November
  • 2018 December
  • 2019 January
  • 2019 February
  • 2019 March
  • 2019 April
  • 2019 May
  • 2019 June
  • 2019 July
  • 2019 August
  • 2019 September
  • 2019 October
  • 2019 November
  • 2019 December
  • 2020 January
  • 2020 February
  • 2020 March
  • 2020 April
  • 2020 May
  • 2020 June
  • 2020 July
  • 2020 August
  • 2020 September
  • 2020 October
  • 2020 November
  • 2020 December
  • 2021 January
  • 2021 February
Silicon Labs
Stay Connected With Us
Plug into the latest on Silicon Labs products, including product releases and resources, documentation updates, PCN notifications, upcoming events, and more.
  • About Us
  • Careers
  • Community
  • Contact Us
  • Corporate Responsibility
  • Privacy and Terms
  • Press Room
  • Investor Relations
  • Site Feedback
  • Cookies
Copyright © Silicon Laboratories. All rights reserved.
粤ICP备15107361号
Also of Interest:
  • Bring Your IoT Designs to Life with Smart,...
  • A Guide to IoT Protocols at Works With...
  • IoT Hero Rainus Enhances the In-Store Shopping...