The General Interest forum is for non-support discussion only. If you have a question about, or need help with a Silicon Labs product, please visit one of the individual product forums.
 

Application engineers do not monitor this forum.
 

View General Interest Board Guidelines ›

我在使用Si5338中,同一端口4个频率进行切换时,循环几个周期,输出波形就中断,单片机还在循环配置Si5338,不知道什么原因。循环输出三个频率就没有问题。

使用的是SSTL输出模式,频率分别为25MHz,100MHz,200MHz,300MHz。每个频率输出时间为100mS。

  • Timing
  • 32-bit MCUs
  • Discussion Forums
Unanswered
  • 请详细描述你的配置过程并提供使用的frequency plan文件。另外,是增加哪一个频率输出时有问题?

    0
  • 所有配置参数使用软件计算的。初始化时设置了所有寄存器,流程使用Si5338数据手册的配置流程。在更改频率时,保持fvco的频率不变,只更改了MultiSynt0和1的相关寄存器52-84。先禁止输出,然后修改寄存器,然后使能输出。在多个频率循环后,就会出现没有频率输出的情况。

     

    0
  • 把200MHz和300MHz去掉就没问题了,搞不懂什么原因。也没超过频率范围,循环过程中会正常一段时间,然后就停止输出了,很困惑。

    0
  • 去掉200Mhz或300Mhz其中一个。

    0
  • Hi

     

    请联系Silabs Timing 中国区 FAE Leo.

     

    email: linquan.luo@silabs.com

    phone: 13794454530.

     

     

    0