The General Interest forum is for non-support discussion only. If you have a question about, or need help with a Silicon Labs product, please visit one of the individual product forums.
 

Application engineers do not monitor this forum.
 

View General Interest Board Guidelines ›

我买个SI5317-EVB开发板,发现输出时钟不准,比如默认设置,说明书上说是10MHZ,测量值是12MHZ

我又试了其他频率,比如按照芯片手册设成38MHZ,测试出来是48MHZ

还有个问题,这个芯片可以微调频率输出,按芯片说明书是给芯片INC或DEC两个管脚发脉冲,可是试了下也没反应

我查了,跳线设置都是按照说明书上做的,应该没问题。

哪位大神用过帮忙解答下啊。

  • Timing
  • 32-bit MCUs
  • Discussion Forums
Unanswered
  • 你好!

    Si5317 是一款去抖时钟,需要你来提供输入信号。比方说你提供一个10MHz抖动很大的时钟输入,Si5317能够去抖然后输出高质量的10MHz时钟信号。如果你需要100MHz的高质量输出时钟,你需要提供一个100MHz的输入信号。当你不提供输入信号时,输出的时钟频率是不准确的。

    请检查:
    1. 你是否提供了与输出时钟相同频率的输入信号
    2. EVB上的LOS1灯是否亮起,表示输入信号有问题
    3. EVB上的LOL灯是否亮起,表示锁相环没有锁定

    如果你需要的是一个任意频率的时钟发生器,可以看看Silabs的Si570和Si514。

    0